iMX6UL HAB Questions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6UL HAB Questions

1,904件の閲覧回数
SJA
Contributor II

Can the signed u-boot image be verified on the EVK without CLOSING the SoC

when loading via USB (mfgtools technique)? When attempting this I

consistently see HAB events with INV_ADDRESS CTX_AUTHENTICATION.

Does the binary CSF file created using the cst tool have to be padded to the

size specified with CONFIG_CSF_SIZE in the u-boot imximage.cfg file before

being appended to the u-boot image?

Does the signed u-boot image need to be padded for 0x1000 alignment?

If so, does the size value specified in the CSF script "[Authenticate Data]

Block =" command reflect the u-boot image size before or after padding?

Note: We are using the HAB4 CSF Fast Authentication loading the images via

USB

ラベル(1)
0 件の賞賛
返信
1 返信

1,477件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Please refer to Appendix E (Freescale manufacturing tool) of

recent AN4581 release (Rev. 1, 10/2015) - how to prepare U-boot for
MFG.

http://cache.freescale.com/files/32bit/doc/app_note/AN4581.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信