iMX6SX framebuffer image rotation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6SX framebuffer image rotation

3,687 Views
texnikk
Contributor III

Q: Does anybody know, how can framebuffer rotation be achieved on iMX6SX cpu, which doesn't have IPU?

Because I've found several threads here regarding image rotation, but looks like all solutions require usage of IPU.

Labels (3)
0 Kudos
Reply
4 Replies

3,315 Views
texnikk
Contributor III

So maybe there are any other solutions?

0 Kudos
Reply

3,315 Views
mtx512
Contributor V

You can use the PXP engine to rotate a buffer and render back to the frame buffer as shown in this example. 

0 Kudos
Reply

3,315 Views
igorpadykov
NXP Employee
NXP Employee

Hi Serhii

one can look at pxp rotation test

pxp_v4l2_test.c\pxp_v4l2_test\test - imx-test - i.MX Driver Test Application Software 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,315 Views
texnikk
Contributor III

Hi igorpadykov,

Thanks for your reply!

Well, actually I need this rotation be performed by framebuffer driver itself, like it was described in i.MX6 IPU and rotating a frame buffer in framebuffer_rotaion_90_degree_kernel_4.9.patch.zip , not from userspace

0 Kudos
Reply