iMX6SX ENET1_RGMII_TXC Description

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6SX ENET1_RGMII_TXC Description

Jump to solution
1,539 Views
vadimaleynikov
Contributor III

Hi,

The IMX6SXRM descibes the ENET1_RGMII_TXC signal as "Serial output Ethernet data. Only valid during TX_EN assertion." in Table 24-1. What is the correct description of the ENET1_RGMII_TXC signal?

Best regards,
Vadim Aleynikov

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,391 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vadim

this is clock which is clocking rgmii data, depicted on

Figure 54. RGMII Transmit Signal Timing Diagram Original i.MX6SX Datasheet

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SXCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,392 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vadim

this is clock which is clocking rgmii data, depicted on

Figure 54. RGMII Transmit Signal Timing Diagram Original i.MX6SX Datasheet

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SXCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply