iMX6SL microSD booting problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6SL microSD booting problem

1,641件の閲覧回数
jiyonghan
Contributor I

Dear All,

I'm HW engineer.

I'd like to get best idea for my issue during my HW debugging.

> I designed my board based on MX6SLEVK.

  Most features are same with reference(MX6SLEVK).

  In MX6SLEVK, SD card boot from SDIO2(J21) port.

  I designed microSD on this SDIO2 instead of SD.

  WP signal was tied to ground.

> My issue is that system was halt on below message.

   galcore: clk_get gpu3d_clk failed, disable 3d!

  Galcore version 5.0.11.25762

  mmc1: error -110 whilst initialising SD card => Error !!

  mmc2: new high speed SDIO card at address 0001

  ALSA device list:

  #0: imx-spdif

  Waiting for root device /dev/mmcblk1p2... => halt on this line

> I compared as below.

   With microSD, I inserted into J21 of MX6SLEVK => Boot ok

                          I wired from J21 pin to microSD connector => same with my issue

                          I wired from 21 to mSD & short WP to ground => Boot ok

   I modified my board based on above results.

   I tied WP signal to ground, but same symptom.

I check whole HW design, but Circuit was same with MX6SLEVK.

> I check SDIO2 Line voltage.

   When booting was ok in MX6SLEVK, SDIO line voltage level is 1.8V

   but Voltage was not correct in my board.

    2pin was 3.3V, other pin was low.

I hope to get best idea to solve my issue if there's any engineer that experienced similar issues.

thanks

BR

Han

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,383件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Han

I would suggest to check also CD signal since it can be used by linux.

Regarding voltages, please test with oscilloscope NVCC33, NVCC18 power

lines of processor.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,383件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

Which BSP you are using?

For 3.0.35, have you modified the iomux for your board?

For the 3.10 and later, have you modified the device tree of iomux for your board?

0 件の賞賛
返信