iMX6Quad GPU AXI BUS Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6Quad GPU AXI BUS Error

1,317 次查看
Salvatore1z
Contributor II

Hello,

I'm using a custom board with an iMX6Quad.

I'm experiancing the following errors (visible through dmesg):

[  414.734840] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x51

[  414.734853] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x51

[  414.746968] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x51

[  414.746990] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x51

[  414.906489] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x51

[  414.906508] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x51

[  414.926427] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x51

[  414.926449] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x51

[  414.930801] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x1

[  414.930818] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x1

[  414.932716] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x51

[  414.932739] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x51

[  414.948729] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x51

[  414.948746] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x51

[  414.954694] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x51

[  414.954717] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x51

[  421.283945] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x1

[  421.284039] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x1

[  421.287336] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x51

[  421.287355] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x51

[  422.366293] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x51

[  422.366321] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x51

[  422.448952] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x1

[  422.448970] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x1

[  422.450486] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x51

[  422.450504] GPU[0]: AXI BUS ERROR, AQAxiStatus=0x51

[  451.963425] [galcore]: GPU[0] hang, automatic recovery.

[  451.963472] [galcore]: recovery done

[  512.083442] [galcore]: GPU[0] hang, automatic recovery.

[  512.083489] [galcore]: recovery done

Any idea about the reasons for such errors?

The problem is not systematic. I'm running a Wayland based HMI.

How do I know the meaning of values reported by AQAxiStatus.

Is there any way to collect more information about this issue?

The Kernel version is 3.14.28.

Thank you.

Salvatore

标签 (3)
标记 (3)
0 项奖励
回复
0 回复数