Hi Sir,
We designed our board with iMX6Q and measured USB client full-speed eye-diagram.
The USB signal voltage level in full-speed cannot reach 3.3V. USB traces impedance is 90 ohm differential controlled.
We tried to increase amplitude with setting register USBPHY1.TX.D_CAL=0x0 by memtool.
The amplitude of full-speed USB signal increase a little but still cannot reach 3.3V. It only has around 2.6V amplitude. (Refer to attached bmp file)
Any other software suggestion ?
Hi Tony1z
available software configuration is given in AN 4589
Configuring USB on i.MX 6 Series Processors sect.4.3.3 Operational settings
http://cache.nxp.com/files/32bit/doc/app_note/AN4589.pdf
If this does not help, it is necessary to look at hardware methods for improving
signal quality.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------