iMX6Q NAND Boot issue in WinCE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6Q NAND Boot issue in WinCE

Jump to solution
9,037 Views
KeshavaGN
Contributor V

Hi all,

I'm trying to boot eboot.nb0 from NAND. (Micron, MT29F4G08ABBDA) in WinCE7.

Processor: i.MX6Q

I have successfully booted u-boot.bin from NAND using kobs-ng tool in linux.

Also, if i use modified eboot.nb0 instead of u-boot.bin in kobs, it is booting without any problem.

But when i use MFGTool (in WinCE) for flashing eboot.nb0, it is not booting.

Following is the nanddump output when i am using kobs (linux) for flashing:

FCB:

0x00000000: 00 00 00 00 00 00 00 00 00 00 00 00 cf fc ff ff

0x00000010: 46 43 42 20 00 00 00 01 50 3c 19 06 00 00 00 00

0x00000020: 00 08 00 00 40 08 00 00 40 00 00 00 00 00 00 00

0x00000030: 00 00 00 00 00 00 00 00 04 00 00 00 00 02 00 00

0x00000040: 00 02 00 00 04 00 00 00 0a 00 00 00 03 00 00 00

0x00000050: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x00000060: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x00000070: 00 00 00 00 00 02 00 00 00 0b 00 00 01 01 00 00

0x00000080: 01 01 00 00 00 01 00 00 cf 07 00 00 00 00 00 00

0x00000090: 00 08 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x000000a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x000000b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x000000c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

DBBT:

0x00080000: 00 ff ff ff ff ff ff ff ff ff 00 00 00 00 44 42

0x00080010: 42 54 00 00 00 01 00 00 00 00 00 00 00 00 00 00

0x00080020: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x00080030: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

and eboot.nb0 at Page 200.

Here, why we are getting first 12 bytes as zeros? (METADATA_SIZE is set to 10). Why two additional zeros?

In WinCE (Using MFGTool):

FCB:

[Metadata: ff ff ff ff ff ff fe ff ff ff ] (only 10 bytes of metadata)

75      b8      fe      ff

46      43      42      20

0       0       0       1

50      3c      19      6

0       0       0       0

0       8       0       0

40      8       0       0

40      0       0       0

0       0       0       0

0       0       0       0

0       0       0       0

4       0       0       0

0       2       0       0

0       2       0       0

4       0       0       0

a       0       0       0

3       0       0       0

0       0       0       0

0       0       0       0

0       0       0       0

0       0       0       0

0       0       0       0

0       0       0       0

0       0       0       0

d8      f9      8a      d9

11      0       0       0

0       2       0       0

40      3       0       0

40      1       0       0

40      1       0       0

0       1       0       0

cf      7       0       0

0       0       0       0

0       8       0       0

0       0       0       0

0       0       0       0

0       0       0       0

0       0       0       0

0       0       0       0

0       0       0       0

0       0       0       0

0       0       0       0

0       0       0       0

0       0       0       0

0       0       0       0

0       0       0       0

0       0       0       0

44      cd      ab      ef

d4      84      a9      ef

ff      ff      ff      ff

ff      ff      ff      ff

ff      ff      ff      ff

DBBT:

0       0       0       0

44      42      42      54

0       0       0       1

0       0       0       0

0       0       0       0

and eboot.nb0 at 200 page.

Following is the nandtype info structure:

//MT29F4G08ABBDAHC

    {

       {NAND, 4096, 2048 * 64, 64, 2048},    //FlashInfo   fi;

       {0x2C, 0xAC, 0x90, 0x15},                    //BYTE        NANDCode[NANDID_LENGTH]

        3,                                          //BYTE        NumBlockCycles

        5,                                          //BYTE        ChipAddrCycleNum

        8,                                          //BYTE        DataWidth

        1,                                          //BYTE        BBMarkNum

        {0},                                        //BYTE        BBMarkPage

        6,                                          //BYTE        StatusBusyBit

        0,                                          //BYTE        StatusErrorBit

        64,                                         //WORD        SpareDataLength

        0x70,                                       //BYTE        CmdReadStatus

        0x00,                                       //BYTE        CmdRead1

        0x30,                                       //BYTE        CmdRead2

        0x90,                                       //BYTE        CmdReadId

        0xff,                                       //BYTE        CmdReset

        0x80,                                       //BYTE        CmdWrite1

        0x10,                                       //BYTE        CmdWrite2

        0x60,                                       //BYTE        CmdErase1

        0xD0,                                       //BYTE        CmdErase2

        {80, 60, 25, 6}                            //NANDTiming  timings

}

Following is the BootBlock structure:

typedef struct _BootBlockStruct_t

{

    UINT32    m_u32Checksum;         //!< First fingerprint in first byte.

    UINT32    m_u32FingerPrint;      //!< 2nd fingerprint at byte 4.

    UINT32    m_u32Version;          //!< 3rd fingerprint at byte 8.

    union

    {

        struct

        {         

            NAND_Timing_t   m_NANDTiming;                   //!< Optimum timing parameters for Tas, Tds, Tdh in nsec.

            UINT32        m_u32Reserved;                  //mx28 needs a dword reservation

         

            UINT32        m_u32DataPageSize;              //!< 2048 for 2K pages, 4096 for 4K pages.

            UINT32        m_u32TotalPageSize;             //!< 2112 for 2K pages, 4314 for 4K pages.

            UINT32        m_u32SectorsPerBlock;           //!< Number of 2K sections per block.

            UINT32        m_u32NumberOfNANDs;             //!< Total Number of NANDs - not used by ROM.

            UINT32        m_u32TotalInternalDie;          //!< Number of separate chips in this NAND.

            UINT32        m_u32CellType;                  //!< MLC or SLC.

            UINT32        m_u32EccBlockNEccType;         //!< Type of ECC, can be one of BCH-0-20

            UINT32        m_u32EccBlock0Size;             //!< Number of bytes for Block0 - BCH

            UINT32        m_u32EccBlockNSize;             //!< Block size in bytes for all blocks other than Block0 - BCH

            UINT32        m_u32EccBlock0EccType;         //!< Ecc level for Block 0 - BCH

            UINT32        m_u32MetadataBytes;             //!< Metadata size - BCH

            UINT32        m_u32NumEccBlocksPerPage;       //!< Number of blocks per page for ROM use - BCH

            UINT32        m_u32EccBlockNEccLevelSDK;      //!< Type of ECC, can be one of BCH-0-20

            UINT32        m_u32EccBlock0SizeSDK;          //!< Number of bytes for Block0 - BCH

            UINT32        m_u32EccBlockNSizeSDK;          //!< Block size in bytes for all blocks other than Block0 - BCH

            UINT32        m_u32EccBlock0EccLevelSDK;      //!< Ecc level for Block 0 - BCH

            UINT32        m_u32NumEccBlocksPerPageSDK;    //!< Number of blocks per page for SDK use - BCH

            UINT32        m_u32MetadataBytesSDK;          //!< Metadata size - BCH

            UINT32        m_u32EraseThreshold;            //!< To set into BCH_MODE register.

            UINT32        m_u32BootPatch;                 //!< 0 for normal boot and 1 to load patch starting next to FCB.

            UINT32        m_u32PatchSectors;              //!< Size of patch in sectors.

            UINT32        m_u32Firmware1_startingSector;  //!< Firmware image starts on this sector.

            UINT32        m_u32Firmware2_startingSector;  //!< Secondary FW Image starting Sector.

            UINT32        m_u32SectorsInFirmware1;        //!< Number of sectors in firmware image.

            UINT32        m_u32SectorsInFirmware2;        //!< Number of sector in secondary FW image.

            UINT32        m_u32DBBTSearchAreaStartAddress;//!< Page address where dbbt search area begins

            UINT32        m_u32BadBlockMarkerByte;        //!< Byte in page data that have manufacturer marked bad block marker, this will

                                                            //!< bw swapped with metadata[0] to complete page data.

            UINT32        m_u32BadBlockMarkerStartBit;    //!< For BCH ECC sizes other than 8 and 16 the bad block marker does not start

                                                            //!< at 0th bit of m_u32BadBlockMarkerByte. This field is used to get to the

                                                            //!< start bit of bad block marker byte with in m_u32BadBlockMarkerByte.

            UINT32        m_u32BBMarkerPhysicalOffset;    //!< FCB value that gives byte offset for bad block marker on physical NAND page.

  UINT32  m_u32BCHType;

  UINT32  m_u32TMTiming2_ReadLatency;

  UINT32  m_u32TMTiming2_PreambleDelay;

  UINT32  m_u32TMTiming2_CEDelay;

  UINT32  m_u32TMTiming2_PostambleDelay;

  UINT32  m_u32TMTiming2_CmdAddPause;

  UINT32  m_u32TMTiming2_DataPause;

  UINT32  m_u32TMSpeed;

  UINT32  m_u32TMTiming1_BusyTimeout;

  UINT32  m_u32DISBBM;

  UINT32  m_u32BBMark_spare_offset;

  UINT32  m_u32Onfi_sync_enable;

  UINT32  m_u32Onfi_sync_speed;

  UINT32  m_u32Onfi_syncNANDData;

  UINT32  m_u32DISBB_Search;

        } FCB_Block;

        struct

        {                         

            UINT32        m_u32NumberBB;                    //!< # Bad Blocks stored in this table for NAND0.

            UINT32        m_u32Number2KPagesBB;           //!< Bad Blocks for NAND0 consume this # of 2K pages.

        } DBBT_Block;

    };

} BootBlockStruct_t;

Following are the values i'm assigning (Which are equal to linux):

FCB

  m_u32FingerPrint = 0x20424346

  m_u32Version = 0x01000000

  m_u32Reserved = 0

  m_NANDTiming.m_u8DataSetup = 80

  m_NANDTiming.m_u8DataHold = 60

  m_NANDTiming.m_u8AddressSetup = 25

  m_NANDTiming.m_u8DSAMPLE_TIME = 6

  m_u32PageDataSize = 2048

  m_u32TotalPageSize = 2112

  m_u32SectorsPerBlock = 64

  m_u32NumberOfNANDs = 0

  m_u32TotalInternalDie = 0

  m_u32CellType = 0

  m_u32EccBlockNEccType = 4

  m_u32EccBlock0Size = 512

  m_u32EccBlockNSize = 512

  m_u32EccBlock0EccType = 4

  m_u32MetadataBytes = 10

  m_u32NumEccBlocksPerPage = 3

  m_u32EccBlockNEccLevelSDK = 0

  m_u32EccBlock0SizeSDK = 0

  m_u32EccBlockNSizeSDK = 0

  m_u32EccBlock0EccLevelSDK = 0

  m_u32NumEccBlocksPerPageSDK = 0

  m_u32MetadataBytesSDK = 0

  m_u32EraseThreshold = 0

  m_u32Firmware1_startingPage = 512

  m_u32Firmware2_startingPage = 2816

  m_u32PagesInFirmware1 = 91

  m_u32PagesInFirmware2 = 91

  m_u32DBBTSearchAreaStartAddress = 256

  m_u32BadBlockMarkerByte = 1999

  m_u32BadBlockMarkerStartBit = 0

  m_u32BBMarkerPhysicalOffset = 2048

  m_u32BCHType = 0

  m_NANDTMTiming.m_u32TMTiming2_ReadLatency = 0

  m_NANDTMTiming.m_u32TMTiming2_PreambleDelay = 0

  m_NANDTMTiming.m_u32TMTiming2_CEDelay = 0

  m_NANDTMTiming.m_u32TMTiming2_PostambleDelay = 0

  m_NANDTMTiming.m_u32TMTiming2_CmdAddPause = 0

  m_NANDTMTiming.m_u32TMTiming2_DataPause = 0

  m_NANDTMTiming.m_u32TMSpeed = 0

  m_NANDTMTiming.m_u32TMTiming1_BusyTimeout = 0

  m_u32DISBBM = 0

DBBT

  m_u32Checksum = 0x00000000

  m_u32FingerPrint = 0x54424244

  m_u32Version = 0x01000000

In WinCE, it is not at all booting.

Where is the mistake?

If metadata size difference is the problem , how i can solve it? ( I have also tried by changing METADATA_SIZE = 12, which increases metadata size, but not booting.)

What are those two extra bytes in linux (kobs)?

Please help.

Thanks.

Regards,

Keshava G N

Labels (4)
1 Solution
7,423 Views
KeshavaGN
Contributor V

Hi,

Solved.

Eboot is booting now.

Correct data to be written for booting:

FCB:

00 00 00 00 00 00 00 00 00 00 00 00 cf fc ff ff
46 43 42 20 00 00 00 01 50 3c 19 06 00 00 00 00
00 08 00 00 40 08 00 00 40 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 04 00 00 00 00 02 00 00
00 02 00 00 04 00 00 00 0a 00 00 00 03 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 02 00 00 00 0b 00 00 01 01 00 00
01 01 00 00 00 01 00 00 cf 07 00 00 00 00 00 00
00 08 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 1b 0c 06 06
10 1f 03 07 00 00 00 1c 0f 17 1f 05 00 00 00 00
00 19 00 00 15 19 00 00 15 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 13 00 00 00 00 16 00 00
00 16 00 00 13 00 00 00 0f 00 00 00 0a 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 16 00 00 00 13 00 00 1c 1c 00 00
1c 1c 00 00 00 1c 00 00 1b 19 00 00 00 00 00 00
00 19 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

DBBT:
00 ff ff ff ff ff ff ff ff ff 00 00 00 00 44 42
42 54 00 00 00 01 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 74 9c 34 5d ed 4b
6d 24 4d 04 d8 e4 48 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

EBOOT:

e5 ff ff ff ff ff ff ff ff ff 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 c2 02 c8 c7 39 aa
0c a8 ef 77 29 f1 78 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 d1 00 20 40 60 74 90 00 00 00 00 00
00 00 00 00 40 74 90 00 00 74 90 00 00 00 00 00
00 00 00 00 d1 00 20 40 00 20 04 80 00 00 00 00
00 00 00 00 54 74 90 00 20 74 90 00 00 00 00 00
00 00 00 00 00 70 90 00 00 10 00 00 01 00 00 00
00 0c 04 80 00 04 08 00 00 0c 04 80 00 04 08 00
00 00 00 00 ff 40 2d e9 00 70 a0 e1 09 06 50 e3
28 30 1f e5 00 30 80 85 18 36 9f e5 00 30 81 85
42 3e a0 e3 00 30 82 85 40 40 4f e2 40 50 4f e2
40 60 4f e2 00 06 9f e5 00 10 e0 e3 68 20 a0 e3
02 10 80 e7 00 10 e0 e3 6c 20 a0 e3 02 10 80 e7
00 10 e0 e3 70 20 a0 e3 02 10 80 e7 00 10 e0 e3
74 20 a0 e3 02 10 80 e7 00 10 e0 e3 78 20 a0 e3
02 10 80 e7 00 10 e0 e3 7c 20 a0 e3 02 10 80 e7
00 10 e0 e3 80 20 a0 e3 02 10 80 e7 00 10 e0 e3
84 20 a0 e3 02 10 80 e7 9c 05 9f e5 9c 15 9f e5
18 20 a0 e3 02 10 80 e7 94 05 9f e5 94 15 9f e5
94 25 9f e5 02 10 80 e7 88 15 9f e5 5b 2e a0 e3
02 10 80 e7 7c 15 9f e5 80 25 9f e5 02 10 80 e7
70 15 9f e5 78 25 9f e5 02 10 80 e7 64 15 9f e5
70 25 9f e5 02 10 80 e7 58 15 9f e5 68 25 9f e5
02 10 80 e7 4c 15 9f e5 60 25 9f e5 02 10 80 e7
40 15 9f e5 17 2d a0 e3 02 10 80 e7 38 10 a0 e3
4c 25 9f e5 02 10 80 e7 38 10 a0 e3 44 25 9f e5
02 10 80 e7 38 10 a0 e3 3c 25 9f e5 02 10 80 e7
38 10 a0 e3 52 2e a0 e3 02 10 80 e7 38 10 a0 e3
28 25 9f e5 02 10 80 e7 38 10 a0 e3 51 2e a0 e3
02 10 80 e7 38 10 a0 e3 14 25 9f e5 02 10 80 e7
38 10 a0 e3 0c 25 9f e5 02 10 80 e7 38 10 a0 e3
04 25 9f e5 02 10 80 e7 00 15 9f e5 00 25 9f e5
02 10 80 e7 38 10 a0 e3 f8 24 9f e5 02 10 80 e7
38 10 a0 e3 f0 24 9f e5 02 10 80 e7 38 10 a0 e3
e8 24 9f e5 2f 4b 52 82 fe b2 58 65 c4 a5 96 f4
3e 02 10 80 e7 38 10 a0 e3 59 2e a0 e3 02 10 80
e7 38 10 a0 e3 d4 24 9f e5 02 10 80 e7 00 10 a0
e3 cc 24 9f e5 02 10 80 e7 38 10 a0 e3 c4 24 9f
e5 02 10 80 e7 38 10 a0 e3 5a 2e a0 e3 02 10 80
e7 38 10 a0 e3 b0 24 9f e5 02 10 80 e7 38 10 a0
e3 a8 24 9f e5 02 10 80 e7 38 10 a0 e3 a0 24 9f
e5 02 10 80 e7 38 10 a0 e3 98 24 9f e5 02 10 80
e7 38 10 a0 e3 7a 2e a0 e3 02 10 80 e7 38 10 a0
e3 84 24 9f e5 02 10 80 e7 38 10 a0 e3 7c 24 9f
e5 02 10 80 e7 38 10 a0 e3 74 24 9f e5 02 10 80
e7 38 10 a0 e3 6c 24 9f e5 02 10 80 e7 02 18 a0
e3 75 2e a0 e3 02 10 80 e7 00 10 a0 e3 58 24 9f
e5 02 10 80 e7 02 18 a0 e3 50 24 9f e5 02 10 80
e7 38 10 a0 e3 48 24 9f e5 02 10 80 e7 02 17 a0
e3 40 24 9f e5 02 10 80 e7 3c 04 9f e5 02 19 a0
e3 1c 10 80 e5 02 19 a0 e3 30 24 9f e5 02 10 80
e7 2c 14 9f e5 5c 18 80 e5 24 14 9f e5 24 24 9f
e5 02 10 80 e7 20 14 9f e5 00 18 80 e5 18 14 9f
e5 12 2b a0 e3 02 10 80 e7 01 15 a0 e3 90 18 80
e5 01 15 a0 e3 04 24 9f e5 02 10 80 e7 00 14 9f
e5 00 24 9f e5 02 10 80 e7 02 1b a0 e3 b8 18 80
e5 02 1b a0 e3 f0 23 9f e5 02 10 80 e7 ec 13 9f
e5 1c 18 80 e5 e4 13 9f e5 20 18 80 e5 e0 13 9f
e5 24 18 80 e5 d4 13 9f e5 28 18 80 e5 d0 13 9f
e5 d0 23 9f e5 02 10 80 e7 c4 13 9f e5 c8 23 9f
e5 02 10 80 e7 b8 13 9f e5 c0 23 9f e5 02 10 80
e7 ac 13 9f e5 b8 23 9f e5 02 10 80 e7 b4 13 9f
e5 2c 18 80 e5 ac 13 9f e5 30 18 80 e5 a4 13 9f
e5 34 18 80 e5 9c 13 9f e5 38 18 80 e5 94 13 9f

.

.

.

Thanks all.

Keshava G N :smileyhappy:

keshavagn@iwavesystems.com

View solution in original post

13 Replies
7,424 Views
KeshavaGN
Contributor V

Hi,

Solved.

Eboot is booting now.

Correct data to be written for booting:

FCB:

00 00 00 00 00 00 00 00 00 00 00 00 cf fc ff ff
46 43 42 20 00 00 00 01 50 3c 19 06 00 00 00 00
00 08 00 00 40 08 00 00 40 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 04 00 00 00 00 02 00 00
00 02 00 00 04 00 00 00 0a 00 00 00 03 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 02 00 00 00 0b 00 00 01 01 00 00
01 01 00 00 00 01 00 00 cf 07 00 00 00 00 00 00
00 08 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 1b 0c 06 06
10 1f 03 07 00 00 00 1c 0f 17 1f 05 00 00 00 00
00 19 00 00 15 19 00 00 15 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 13 00 00 00 00 16 00 00
00 16 00 00 13 00 00 00 0f 00 00 00 0a 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 16 00 00 00 13 00 00 1c 1c 00 00
1c 1c 00 00 00 1c 00 00 1b 19 00 00 00 00 00 00
00 19 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

DBBT:
00 ff ff ff ff ff ff ff ff ff 00 00 00 00 44 42
42 54 00 00 00 01 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 74 9c 34 5d ed 4b
6d 24 4d 04 d8 e4 48 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

EBOOT:

e5 ff ff ff ff ff ff ff ff ff 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 c2 02 c8 c7 39 aa
0c a8 ef 77 29 f1 78 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 d1 00 20 40 60 74 90 00 00 00 00 00
00 00 00 00 40 74 90 00 00 74 90 00 00 00 00 00
00 00 00 00 d1 00 20 40 00 20 04 80 00 00 00 00
00 00 00 00 54 74 90 00 20 74 90 00 00 00 00 00
00 00 00 00 00 70 90 00 00 10 00 00 01 00 00 00
00 0c 04 80 00 04 08 00 00 0c 04 80 00 04 08 00
00 00 00 00 ff 40 2d e9 00 70 a0 e1 09 06 50 e3
28 30 1f e5 00 30 80 85 18 36 9f e5 00 30 81 85
42 3e a0 e3 00 30 82 85 40 40 4f e2 40 50 4f e2
40 60 4f e2 00 06 9f e5 00 10 e0 e3 68 20 a0 e3
02 10 80 e7 00 10 e0 e3 6c 20 a0 e3 02 10 80 e7
00 10 e0 e3 70 20 a0 e3 02 10 80 e7 00 10 e0 e3
74 20 a0 e3 02 10 80 e7 00 10 e0 e3 78 20 a0 e3
02 10 80 e7 00 10 e0 e3 7c 20 a0 e3 02 10 80 e7
00 10 e0 e3 80 20 a0 e3 02 10 80 e7 00 10 e0 e3
84 20 a0 e3 02 10 80 e7 9c 05 9f e5 9c 15 9f e5
18 20 a0 e3 02 10 80 e7 94 05 9f e5 94 15 9f e5
94 25 9f e5 02 10 80 e7 88 15 9f e5 5b 2e a0 e3
02 10 80 e7 7c 15 9f e5 80 25 9f e5 02 10 80 e7
70 15 9f e5 78 25 9f e5 02 10 80 e7 64 15 9f e5
70 25 9f e5 02 10 80 e7 58 15 9f e5 68 25 9f e5
02 10 80 e7 4c 15 9f e5 60 25 9f e5 02 10 80 e7
40 15 9f e5 17 2d a0 e3 02 10 80 e7 38 10 a0 e3
4c 25 9f e5 02 10 80 e7 38 10 a0 e3 44 25 9f e5
02 10 80 e7 38 10 a0 e3 3c 25 9f e5 02 10 80 e7
38 10 a0 e3 52 2e a0 e3 02 10 80 e7 38 10 a0 e3
28 25 9f e5 02 10 80 e7 38 10 a0 e3 51 2e a0 e3
02 10 80 e7 38 10 a0 e3 14 25 9f e5 02 10 80 e7
38 10 a0 e3 0c 25 9f e5 02 10 80 e7 38 10 a0 e3
04 25 9f e5 02 10 80 e7 00 15 9f e5 00 25 9f e5
02 10 80 e7 38 10 a0 e3 f8 24 9f e5 02 10 80 e7
38 10 a0 e3 f0 24 9f e5 02 10 80 e7 38 10 a0 e3
e8 24 9f e5 2f 4b 52 82 fe b2 58 65 c4 a5 96 f4
3e 02 10 80 e7 38 10 a0 e3 59 2e a0 e3 02 10 80
e7 38 10 a0 e3 d4 24 9f e5 02 10 80 e7 00 10 a0
e3 cc 24 9f e5 02 10 80 e7 38 10 a0 e3 c4 24 9f
e5 02 10 80 e7 38 10 a0 e3 5a 2e a0 e3 02 10 80
e7 38 10 a0 e3 b0 24 9f e5 02 10 80 e7 38 10 a0
e3 a8 24 9f e5 02 10 80 e7 38 10 a0 e3 a0 24 9f
e5 02 10 80 e7 38 10 a0 e3 98 24 9f e5 02 10 80
e7 38 10 a0 e3 7a 2e a0 e3 02 10 80 e7 38 10 a0
e3 84 24 9f e5 02 10 80 e7 38 10 a0 e3 7c 24 9f
e5 02 10 80 e7 38 10 a0 e3 74 24 9f e5 02 10 80
e7 38 10 a0 e3 6c 24 9f e5 02 10 80 e7 02 18 a0
e3 75 2e a0 e3 02 10 80 e7 00 10 a0 e3 58 24 9f
e5 02 10 80 e7 02 18 a0 e3 50 24 9f e5 02 10 80
e7 38 10 a0 e3 48 24 9f e5 02 10 80 e7 02 17 a0
e3 40 24 9f e5 02 10 80 e7 3c 04 9f e5 02 19 a0
e3 1c 10 80 e5 02 19 a0 e3 30 24 9f e5 02 10 80
e7 2c 14 9f e5 5c 18 80 e5 24 14 9f e5 24 24 9f
e5 02 10 80 e7 20 14 9f e5 00 18 80 e5 18 14 9f
e5 12 2b a0 e3 02 10 80 e7 01 15 a0 e3 90 18 80
e5 01 15 a0 e3 04 24 9f e5 02 10 80 e7 00 14 9f
e5 00 24 9f e5 02 10 80 e7 02 1b a0 e3 b8 18 80
e5 02 1b a0 e3 f0 23 9f e5 02 10 80 e7 ec 13 9f
e5 1c 18 80 e5 e4 13 9f e5 20 18 80 e5 e0 13 9f
e5 24 18 80 e5 d4 13 9f e5 28 18 80 e5 d0 13 9f
e5 d0 23 9f e5 02 10 80 e7 c4 13 9f e5 c8 23 9f
e5 02 10 80 e7 b8 13 9f e5 c0 23 9f e5 02 10 80
e7 ac 13 9f e5 b8 23 9f e5 02 10 80 e7 b4 13 9f
e5 2c 18 80 e5 ac 13 9f e5 30 18 80 e5 a4 13 9f
e5 34 18 80 e5 9c 13 9f e5 38 18 80 e5 94 13 9f

.

.

.

Thanks all.

Keshava G N :smileyhappy:

keshavagn@iwavesystems.com

7,423 Views
leoyanfeng
Contributor II

Hi Keshava G N:

     Sorry for my poor english.

     Can you share the detail about your solution.

     I am trying to booting eboot from nand too.Thank you very much.

//write NCB to block 0/2

    memset(&NCB, 0, sizeof(NCB));

    memset(sectorBuf, 0x00, NANDFC_BOOT_SIZE);

    NCB.m_u32FingerPrint = 0x20424346;

    NCB.m_u32Version = 0x01000000;

    NCB.FCB_Block.m_NANDTiming.initializer = 0x140A050A;

    NCB.FCB_Block.m_u32DataPageSize = pFlashInfo->fi.wDataBytesPerSector;

    NCB.FCB_Block.m_u32TotalPageSize = pFlashInfo->fi.wDataBytesPerSector + pFlashInfo->SpareDataLength;

    NCB.FCB_Block.m_u32SectorsPerBlock = pFlashInfo->fi.wSectorsPerBlock;

  

// Not Use By Rom

    //NCB.FCB_Block.m_u32NumberOfNANDs = pFlashInfo->NumberOfChip;

    // Not Use By Rom   

//NCB.FCB_Block.m_u32TotalInternalDie = 1;

    // Not Use By Rom   

//NCB.FCB_Block.m_u32CellType = 1;

   

    if(pFlashInfo->fi.wDataBytesPerSector == 2048)

    {

        NCB.FCB_Block.m_u32EccBlockNEccType = ECCN_2K64_PAGE;

    }

    else if(pFlashInfo->fi.wDataBytesPerSector == 4096 && pFlashInfo->SpareDataLength == 128)

    {

        NCB.FCB_Block.m_u32EccBlockNEccType = ECCN_4K128_PAGE;

    }

    else if(pFlashInfo->fi.wDataBytesPerSector == 4096 && pFlashInfo->SpareDataLength == 218)

    {

        NCB.FCB_Block.m_u32EccBlockNEccType = ECCN_4K218_PAGE;

    }

    else if(pFlashInfo->fi.wDataBytesPerSector == 8192 && pFlashInfo->SpareDataLength == 448)

    {

        NCB.FCB_Block.m_u32EccBlockNEccType = ECCN_8K_448_ONFI_PAGE;

    }

    else

    {

        RETAILMSG(1, (_T("Fatal Error!\r\n")));

        return FALSE;

    }

    NCB.FCB_Block.m_u32EccBlock0EccType = ECC0_2K4K_PAGE;//!< Ecc level for Block 0 - BCH
NCB.FCB_Block.m_u32EccBlock0Size = 0;//!< Number of bytes for Block0 - BCH
    NCB.FCB_Block.m_u32EccBlockNSize = 512;//!< Block size in bytes for all blocks other than Block0 - BCH

    NCB.FCB_Block.m_u32NumEccBlocksPerPage = pFlashInfo->fi.wDataBytesPerSector / 512;   //!< Number of blocks per page - BCH

    NCB.FCB_Block.m_u32MetadataBytes = METADATA_SIZE;//!< Metadata size - BCH

    // Not Use By Rom

//NCB.FCB_Block.m_u32EraseThreshold = NCB.FCB_Block.m_u32EccBlockNEccType;

NCB.FCB_Block.m_u32BCHType = 0; 

    if(pFlashInfo->fi.wDataBytesPerSector == 8192 && pFlashInfo->SpareDataLength == 448)

    {

        NCB.FCB_Block.m_u32EccBlock0EccType = ECC0_8K_448_ONFI_PAGE;//!< Ecc level for Block 0 - BCH
        NCB.FCB_Block.m_u32EccBlock0Size = 1024;//!< Number of bytes for Block0 - BCH
        NCB.FCB_Block.m_u32EccBlockNSize = 1024;//!< Block size in bytes for all blocks other than Block0 - BCH

        NCB.FCB_Block.m_u32NumEccBlocksPerPage = pFlashInfo->fi.wDataBytesPerSector / 1024 - 1;  //!< Number of blocks per page - BCH

        NCB.FCB_Block.m_u32MetadataBytes = METADATA_SIZE;//!< Metadata size - BCH

        NCB.FCB_Block.m_u32EraseThreshold = NCB.FCB_Block.m_u32EccBlockNEccType;

        NCB.FCB_Block.m_u32BCHType = 1; 

    }

    if(!GetGoodPhyBlock(IMAGE_BOOT_BOOTIMAGE_NAND_OFFSET, &startBlk1) || \

    !GetGoodPhyBlock(IMAGE_BOOT_BOOTIMAGE_NAND_OFFSET + IMAGE_BOOT_BOOTIMAGE_NAND_BLOCKS / 2, &startBlk2) || \

    !GetGoodPhyBlock(IMAGE_BOOT_BOOTIMAGE_NAND_OFFSET + IMAGE_BOOT_BOOTIMAGE_NAND_BLOCKS, &endBlk2) || \

    !GetGoodPhyBlock(IMAGE_BOOT_DBBT_NAND_OFFSET, &bbtBlk))

    {

        RETAILMSG(TRUE, (_T(" get good block failed\r\n")));

        return FALSE;

    }

    NCB.FCB_Block.m_u32Firmware1_startingSector = startBlk1 * pFlashInfo->fi.wSectorsPerBlock;//!< Firmware image starts on this sector.
    NCB.FCB_Block.m_u32SectorsInFirmware1 = (startBlk2 - startBlk1) * pFlashInfo->fi.wSectorsPerBlock;//!< Number of sectors in firmware image.
    NCB.FCB_Block.m_u32Firmware2_startingSector = startBlk2 * pFlashInfo->fi.wSectorsPerBlock;//!< Secondary FW Image starting Sector.
    NCB.FCB_Block.m_u32SectorsInFirmware2 = (endBlk2 - startBlk2) * pFlashInfo->fi.wSectorsPerBlock;//!< Number of sector in secondary FW image.

    NCB.FCB_Block.m_u32DBBTSearchAreaStartAddress = bbtBlk * pFlashInfo->fi.wSectorsPerBlock;

   

    if(pFlashInfo->fi.wDataBytesPerSector == 2048)

    {

        NCB.FCB_Block.m_u32BadBlockMarkerByte = BBMarkByteOffsetInPageData_2K64;

        NCB.FCB_Block.m_u32BadBlockMarkerStartBit = BBMarkBitOffset_2K64;

    }

    else if(pFlashInfo->fi.wDataBytesPerSector == 4096 && pFlashInfo->SpareDataLength == 128)

    {

        NCB.FCB_Block.m_u32BadBlockMarkerByte = BBMarkByteOffsetInPageData_4K128;

        NCB.FCB_Block.m_u32BadBlockMarkerStartBit = BBMarkBitOffset_4K128;

    }

    else if(pFlashInfo->fi.wDataBytesPerSector == 4096 && pFlashInfo->SpareDataLength == 218)

    {

        NCB.FCB_Block.m_u32BadBlockMarkerByte = BBMarkByteOffsetInPageData_4K218;

        NCB.FCB_Block.m_u32BadBlockMarkerStartBit = BBMarkBitOffset_4K218;

    }

    else if(pFlashInfo->fi.wDataBytesPerSector == 8192 && pFlashInfo->SpareDataLength == 448)

    {

        NCB.FCB_Block.m_u32BadBlockMarkerByte = BBMarkByteOffsetInPageData_8K448;

        NCB.FCB_Block.m_u32BadBlockMarkerStartBit = BBMarkBitOffset_8K448;

    }

   

    NCB.FCB_Block.m_u32BBMarkerPhysicalOffset = pFlashInfo->fi.wDataBytesPerSector;

    NCB.FCB_Block.m_u32DISBBM = 0;

    NCB.FCB_Block.m_u32BBMarkSpareOffset = 0;

    //For Toggle NAND

    if(g_CSPfi.ToggleNand)

    {

        NCB.FCB_Block.m_ToggleModeNANDData.m_u32ReadLatency = g_ToggleNandInfo.NandTiming2.byReadLatency;

        NCB.FCB_Block.m_ToggleModeNANDData.m_u32PreambleDelay = g_ToggleNandInfo.NandTiming2.byPreambleDelay;

        NCB.FCB_Block.m_ToggleModeNANDData.m_u32CEDelay = g_ToggleNandInfo.NandTiming2.byCeDelay;

        NCB.FCB_Block.m_ToggleModeNANDData.m_u32PostambleDelay = g_ToggleNandInfo.NandTiming2.byPostambleDelay;

        NCB.FCB_Block.m_ToggleModeNANDData.m_u32CmdAddPause = g_ToggleNandInfo.NandTiming2.byCmdAddPause;

        NCB.FCB_Block.m_ToggleModeNANDData.m_u32DataPause = g_ToggleNandInfo.NandTiming2.byDataPause;

        NCB.FCB_Block.m_ToggleModeNANDData.m_u32ToggleModeSpeed = 0;

        NCB.FCB_Block.m_ToggleModeNANDData.m_u32BusyTimeout = g_ToggleNandInfo.NandTiming1.wDeviceBusyTimeout;

    }

    memcpy(sectorBuf + NAND_HC_ECC_OFFSET_DATA_COPY, &NCB, sizeof(NCB));

    NCB.m_u32Checksum = GetBCBChecksum(sectorBuf + NAND_HC_ECC_OFFSET_DATA_COPY + 4, 512 - 4);

    memcpy(sectorBuf + NAND_HC_ECC_OFFSET_DATA_COPY, &NCB, sizeof(NCB));

   

    CalculateHammingForNCB_New((unsigned char *)sectorBuf + NAND_HC_ECC_OFFSET_DATA_COPY, sectorBuf + NAND_HC_ECC_OFFSET_PARITY_COPY, NAND_HC_ECC_SIZEOF_DATA_BLOCK_IN_BYTES);

   

    memset(&si, 0x00, sizeof(SectorInfo));

    //si.bOEMReserved = (BYTE)(~OEM_BLOCK_RESERVED);

0 Kudos
Reply
7,423 Views
KeshavaGN
Contributor V

HuangShijie , FlorentAuger , terry_lr :



Please help: iMX6Q NAND Boot issue in WinCE

Thanks.

Regards,

Keshava G N

7,423 Views
andrew_questps
Contributor III

One point would be that the image you use in the MfgTool needs to know about the flash you are using, so I had to recompile the UUT versions of WinCE with the correct flash selected.

There was also an issue with FMD_Init where it didn't reconfigure it's details once you had used the lookup table, a couple of the values were defaulting to the #defines for a specific nand chip. I had to add the call CSPNAND_Init again once Eboot had run through the lookup table in Nandtypes.h or it was messing around with the bad block tables.

7,423 Views
KeshavaGN
Contributor V

Hi Webster,

Following is my FMD_Init function:

PVOID FMD_Init(LPCTSTR lpActiveReg, PPCI_REG_INFO pRegIn, PPCI_REG_INFO pRegOut)

{

    DWORD i, j;

    PVOID pResult;

    DWORD FullCode;

  

    UNREFERENCED_PARAMETER(lpActiveReg);

    UNREFERENCED_PARAMETER(pRegIn);

    UNREFERENCED_PARAMETER(pRegOut);

  

    // 0. Setup global variables. Also may add more software logic here in future

    memset(&g_FlashInfoExt, 0, sizeof(g_FlashInfoExt));

    BSPNAND_GetFlashInfo(&g_FlashInfoExt);

  

    // 1. initial hardware

    if(g_FlashInfoExt.AutoDec.Enable)

    {

        g_FlashInfoExt.CmdReset = 0xff;

        g_FlashInfoExt.CmdReadId = 0x90;

    }

  

    pResult = CSPNAND_Init(&g_FlashInfoExt);

    if(pResult == NULL)

    {

        goto cleanUp;

    }

  

    // 2. Auto detect NAND chip if it's enabled

    if(g_FlashInfoExt.AutoDec.Enable)

    {

        g_FlashInfoExt.NumberOfChip = 0;

        //BSP enables auto detect mode

        for(i = 0; i < g_FlashInfoExt.AutoDec.CsSearchRange; i++)

        {

            CSPNAND_Reset(i);

            FullCode = CSPNAND_ReadID(i);

            //only support multi-nand with same type

            //only support multi-nand connected continously

            for(j = 0; j < sizeof(ChipInfo)/sizeof(ChipInfo[0]); j++)

            {

                if(!memcmp(&FullCode, ChipInfo[j].NANDCode, sizeof(FullCode)))

                {

                    //Quit the loop

                    //i = g_FlashInfoExt.AutoDec.CsSearchRange;

                    DEBUGMSG(TRUE, (_T("NAND ID=0x%x\r\n"),FullCode));

                  

                    g_FlashInfoExt.NumberOfChip++;

                    if(g_FlashInfoExt.NumberOfChip == 1)

                    {

                        memcpy(&g_FlashInfoExt, &ChipInfo[j], sizeof(NandChipInfo));

  g_FlashInfoExt.SpareDataLength = 64;

  g_FlashInfoExt.StatusBusyBit = 6;


                        g_FlashInfoExt.BBMarkPage = ChipInfo[j].BBMarkPage;

                    }

                    break;

                }

            }

        }

        if(!g_FlashInfoExt.NumberOfChip)

        {

            ERRORMSG(TRUE, (_T("No NAND type matched!\r\n")));

            return FALSE;  

        }

    }

    else

    {

        for(i = 0; i < g_FlashInfoExt.NumberOfChip; i++)

        {

            CSPNAND_Reset(i);

            if((WORD)CSPNAND_ReadID(i) != g_FlashInfoExt.NANDIDCode)

            {

                pResult = NULL;

                goto cleanUp;

            }

        }

    }

//PostInit:

    RETAILMSG(TRUE, (_T("NumberOfChip=%d\r\n"),g_FlashInfoExt.NumberOfChip));

    CSPNAND_PostInit(&g_FlashInfoExt);

    if(g_FlashInfoExt.ILSupport && CSPNAND_ILSupport())

    {

        //silicon supports interleave mode & bsp needs interleave mode

        g_bInterLeaveMode = TRUE;

    }

    if(!BBT_Init())

    {

        RETAILMSG(TRUE, (TEXT("InitializeBBT Fail\r\n")));

    }

cleanUp:

    return pResult;

}

Whether this is correct?

Thanks. :smileyhappy:

With regards,

Keshava G N

7,423 Views
andrew_questps
Contributor III

PVOID FMD_Init(LPCTSTR lpActiveReg, PPCI_REG_INFO pRegIn, PPCI_REG_INFO pRegOut)

{

    DWORD i, j;

    PVOID pResult;

    DWORD FullCode, TempCode;

    UNREFERENCED_PARAMETER(lpActiveReg);

    UNREFERENCED_PARAMETER(pRegIn);

    UNREFERENCED_PARAMETER(pRegOut);

    // 0. Setup global variables. Also may add more software logic here in future

    memset(&g_FlashInfoExt, 0, sizeof(g_FlashInfoExt));

    BSPNAND_GetFlashInfo(&g_FlashInfoExt);

    pResult = CSPNAND_Init(&g_FlashInfoExt);

    if(pResult == NULL)

    {

        RETAILMSG(TRUE, (_T("FMD_Init failed\r\n")));

        goto cleanUp;

    }

    // 2. Auto detect NAND chip if it's enabled

    if(g_FlashInfoExt.AutoDec.Enable)

    {

        g_FlashInfoExt.NumberOfChip = 0;

        // BSP enables auto detect mode

        for(i = 0; i < g_FlashInfoExt.AutoDec.CsSearchRange; i++)

        {

            CSPNAND_Reset(i);

            FullCode = CSPNAND_ReadID(i);

            RETAILMSG(TRUE, (_T("FMD_Init %X\r\n"), FullCode));

            // only support multi-nand with same type

            // only support multi-nand connected continously

            for(j = 0; j < sizeof(ChipInfo)/sizeof(ChipInfo[0]); j++)

            {

                memcpy(&TempCode, ChipInfo[j].NANDCode, sizeof(ChipInfo[j].NANDCode));

                if(!memcmp(&FullCode, ChipInfo[j].NANDCode, sizeof(FullCode)))

                {

                    DEBUGMSG(TRUE, (_T("FMD_Init(%d), %d, (%d,%d)\r\n"), j,

                        ChipInfo[j].BBMarkNum, ChipInfo[j].BBMarkPage[0],

                        ChipInfo[j].BBMarkNum == 2

                        ? ChipInfo[j].BBMarkPage[1] : 0));

                    g_FlashInfoExt.NumberOfChip++;

                    if(g_FlashInfoExt.NumberOfChip == 1)

                    {

                        memcpy(&g_FlashInfoExt, &ChipInfo[j], sizeof(NandChipInfo));

                        g_FlashInfoExt.BBMarkNum = ChipInfo[j].BBMarkNum;

                        memcpy(g_FlashInfoExt.BBMarkPage, ChipInfo[j].BBMarkPage, sizeof(ChipInfo[j].BBMarkPage));

                        g_FlashInfoExt.ChipInfo.BBMarkNum = ChipInfo[j].BBMarkNum;

                        memcpy(g_FlashInfoExt.ChipInfo.BBMarkPage, ChipInfo[j].BBMarkPage, sizeof(ChipInfo[j].BBMarkPage));

                    }

                    break;

                }

                else if(j == (sizeof(ChipInfo)/sizeof(ChipInfo[0]) - 1))

                {

                    if(!g_FlashInfoExt.NumberOfChip)

                    {

                        ERRORMSG(TRUE, (_T("no NAND type matched!\r\n")));

                        return FALSE;

                    }

                    goto PostInit;

                }

            }

        }

    }

    else

    {

        for(i = 0; i < g_FlashInfoExt.NumberOfChip; i++)

        {

            CSPNAND_Reset(i);

            if((WORD)CSPNAND_ReadID(i) != g_FlashInfoExt.NANDIDCode)

            {

                DEBUGMSG(TRUE, (_T("CSPNAND_ReadID(%X) != %X\r\n"), (WORD)CSPNAND_ReadID(i), g_FlashInfoExt.NANDIDCode));

                pResult = NULL;

                goto cleanUp;

            }

        }

    }

PostInit:

    DEBUGMSG(TRUE, (_T("NumberOfChip=%d\r\n"), g_FlashInfoExt.NumberOfChip));

    DEBUGMSG(TRUE, (_T("BBIMainAddr=%d\r\n"), g_FlashInfoExt.BBIMainAddr));

   DEBUGMSG(TRUE, (_T("NumBlockCycles=%d\r\n"), g_FlashInfoExt.NumBlockCycles));

    DEBUGMSG(TRUE, (_T("ChipAddrCycleNum=%d\r\n"), g_FlashInfoExt.ChipAddrCycleNum));

    DEBUGMSG(TRUE, (_T("dwBytesPerBlock=%d\r\n"), g_FlashInfoExt.fi.dwBytesPerBlock));

    DEBUGMSG(TRUE, (_T("dwNumBlocks=%d\r\n"), g_FlashInfoExt.fi.dwNumBlocks));

    DEBUGMSG(TRUE, (_T("wDataBytesPerSector=%d\r\n"), g_FlashInfoExt.fi.wDataBytesPerSector));

    DEBUGMSG(TRUE, (_T("wSectorsPerBlock=%d\r\n"), g_FlashInfoExt.fi.wSectorsPerBlock));

    DEBUGMSG(TRUE, (_T("BBMarkNum=%d\r\n"), g_FlashInfoExt.ChipInfo.BBMarkNum));

    DEBUGMSG(TRUE, (_T("BBMarkPage1=%d\r\n"), g_FlashInfoExt.ChipInfo.BBMarkPage[0]));

    if (g_FlashInfoExt.ChipInfo.BBMarkNum > 1)

    {

        DEBUGMSG(TRUE, (_T("BBMarkPage2=%d\r\n"), g_FlashInfoExt.ChipInfo.BBMarkPage[1]));

    }

CSPNAND_PostInit(&g_FlashInfoExt);

// ensure we are using the new values.

    pResult = CSPNAND_Init(&g_FlashInfoExt);

    if(pResult == NULL)

    {

        RETAILMSG(TRUE, (_T("CSPNAND_PostInit failed\r\n")));

        goto cleanUp;

    }

    if(g_FlashInfoExt.ILSupport && CSPNAND_ILSupport())

    {

        //silicon supports interleave mode & bsp needs interleave mode

        g_bInterLeaveMode = TRUE;

    }

    if(!BBT_Init())

    {

        RETAILMSG(TRUE, (TEXT("InitializeBBT Fail\r\n")));

    }

cleanUp:

    return pResult;

}

That is my new FMD_Init. I also have to support a flash that uses 2 bad block table blocks - ie BBMarkNum = 2 which is why I have the extra debug.

7,423 Views
KeshavaGN
Contributor V

Hi Webster,

I ensured that my NAND flash values are updating.

Now, while comparing the data written in NAND (ie: FCB and DBBT) in linux and in WinCE, i am doubting on ECC values written using WinCE.

Can you post the ECC calculation procedure in your code?

Thanks .

With regards,

Keshava G N

7,423 Views
andrew_questps
Contributor III

I haven't had to change anything to do with the ECC calculation as my chip only uses 4-bit ECC.

7,423 Views
KeshavaGN
Contributor V

Hi Webster,

Do you know how (and where in source code) "metadata" is written in NAND?

Can we edit it?

Thanks.

With regards,

Keshava G N

7,423 Views
HuangShijie
Contributor III

The metadata is written with the first data chunk(most of the time, it's 512bytes).

You can write some data in the metadata, but after you have written the metadata to nand, you can not change it any more.

Of course, if you erase the block again, you can write some other data to the metadata again.

7,423 Views
KeshavaGN
Contributor V

Hi HuangShijie ,

Thanks...

Do you have any idea about my issue: iMX6Q NAND Boot issue in WinCE

Thanks.

Regards,

Keshava G N

7,423 Views
KeshavaGN
Contributor V

Hi Webster,

Thank you for your help... :smileyhappy:

With regards,

Keshava G N

7,423 Views
KeshavaGN
Contributor V

Hi Webster,

Thanks for quick response.

Andre Webster wrote:

One point would be that the image you use in the MfgTool needs to know about the flash you are using, so I had to recompile the UUT versions of WinCE with the correct flash selected.

I'm using the updated image.

Andre Webster wrote:

There was also an issue with FMD_Init where it didn't reconfigure it's details once you had used the lookup table, a couple of the values were defaulting to the #defines for a specific nand chip. I had to add the call CSPNAND_Init again once Eboot had run through the lookup table in Nandtypes.h or it was messing around with the bad block tables.

Please tell me more about this issue.

Which values are causing problem? and where i have to add call to CSPNAND_Init ?

Thanks.

With regards,

Keshava G N