iMX6Q Android spdif and sgtl5000 output at same time?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6Q Android spdif and sgtl5000 output at same time?

1,222件の閲覧回数
tsaiderek
Contributor II

Hello,

We porting Android4.3 JB on custom board,

and desired output two channel at the same time (sgtl5000 & spdif)

on config_sgtl5000.h

static struct audio_card sgtl5000_card ={

  .name = "sgtl5000-audio",

  .driver_name = "sgtl5000-audio",

  .supported_out_devices=

      AUDIO_DEVICE_OUT_SPEAKER|

      AUDIO_DEVICE_OUT_WIRED_HEADPHONE|

      AUDIO_DEVICE_OUT_DEFAULT|

on config_spdif.h

static struct audio_card spdif_card ={

  .name = "imx-spdif",

  .driver_name = "imx-spdif",

  .supported_out_devices=

      AUDIO_DEVICE_OUT_AUX_DIGITAL,

when boot device

sgtl5000 1-000a: sgtl5000 revision 17

asoc: sgtl5000 <-> imx-ssi.1 mapping ok

asoc: mxc-spdif <-> imx-spdif-dai.0 mapping ok

ALSA device list:

  #0: sgtl5000-audio

  #1: imx-spdif

and we can use tinyplay test output

tinyplay a.wav -D 0 -> sgtl5000 output audio

tinyplay a.wav -D 1 -> spdif output audio

and it's fine !

when we define audio_policy.conf

global_configuration {

  attached_output_devices AUDIO_DEVICE_OUT_SPEAKER

  default_output_device AUDIO_DEVICE_OUT_SPEAKER

  attached_input_devices AUDIO_DEVICE_IN_BUILTIN_MIC

}

Default channel is sgtl5000

and

global_configuration {

  attached_output_devices AUDIO_DEVICE_OUT_AUX_DIGITAL

  default_output_device AUDIO_DEVICE_OUT_AUX_DIGITAL

  attached_input_devices AUDIO_DEVICE_IN_BUILTIN_MIC

}

Default channel is spdif

how to output two channel audio at the same time?

Thanks.

ラベル(3)
0 件の賞賛
返信
1 返信

823件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Tsai,

We have try to get two audio outputs on Android 4.3 without success we believe it is a limitation of the Android framework.  since if you try separately every  output it is working fine.

0 件の賞賛
返信