iMX6DQ : EIM byte access on 16bit Data-bus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX6DQ : EIM byte access on 16bit Data-bus

跳至解决方案
1,152 次查看
koichisakagami
Contributor II

Dear community,

We have a question about EIM byte access.

The EIM is configured for 16-bit Non Multiplexed Address/Data mode communication [ DSZ=010, MUM=0].

    Address_bus : EIM_AD[15:0]
    Address_bus : EIM_ADDR[25:16]
    Data_bus       :EIM_DATA[23:16] - EIM_EB2_B
    Data_bus       :EIM_DATA[31:24] - EIM_EB3_B

[Question]


When we execute the " byte write access" to EIM ,
which data bus is used ?

Best Regards,
Koichi Sakagami

标签 (1)
0 项奖励
回复
1 解答
1,028 次查看
Yuri
NXP Employee
NXP Employee

Hello,

For even bytes - EB2 is asserted ; for odd bytes - EB3.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,029 次查看
Yuri
NXP Employee
NXP Employee

Hello,

For even bytes - EB2 is asserted ; for odd bytes - EB3.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复