iMX6DL kernel panic issue when using CSR Wifi driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6DL kernel panic issue when using CSR Wifi driver

Jump to solution
3,443 Views
jianxingwang
Contributor II

Hi

Thank you for support.

We found a kernel panic issue when using CSR wifi driver with our iMX6D platform which runing the OS version as 3.0.35.

Currently we have no idea about this issue, So i copied the crash stack in the following, Hope anyone can help me for this

panic.

<3>[  587.015209] unifi3: unifi_receive_event: Received MaPacketInd with status 4, Frame dropped

<3>[  587.024654] unifi3: unifi_receive_event: Received MaPacketInd with status 4, Frame dropped

<5>[  587.243559] (!!) init: starting 'dhcpcd_wlan0'

<3>[  597.575232] unifi3: unifi_receive_event: Received MaPacketInd with status 4, Frame dropped

<7>[  598.096879] wlan0: no IPv6 routers present

<3>[  600.233547] unifi3: unifi_receive_event: Received MaPacketInd with status 4, Frame dropped

<3>[  600.243102] unifi3: unifi_receive_event: Received MaPacketInd with status 4, Frame dropped

<5>[  607.450101] (!!) init: service 'dhcpcd_wlan0' is being stopped

<6>[  607.498092] (II) init: waitpid returned pid 3780, status = 00000100

<5>[  607.504636] (!!) init: process 'dhcpcd_wlan0', pid 3780 exited

<5>[  607.689298] (!!) init: starting 'dhcpcd_wlan0'

<4>[  617.422335] TouchPanel receive response in 5s, jiffies: 31623.

<7>[  618.286881] wlan0: no IPv6 routers present

<5>[  623.767481] (!!) init: service 'dhcpcd_wlan0' is being stopped

<6>[  623.789368] (II) init: waitpid returned pid 3789, status = 00000100

<5>[  623.821959] (!!) init: process 'dhcpcd_wlan0', pid 3789 exited

<5>[  628.642811] (!!) init: starting 'dhcpcd_wlan0'

<7>[  639.946883] wlan0: no IPv6 routers present

<4>[  642.424971] TouchPanel receive response in 5s, jiffies: 34123.

<5>[  648.844763] (!!) init: service 'dhcpcd_wlan0' is being stopped

<6>[  648.888080] (II) init: waitpid returned pid 3805, status = 00000100

<5>[  648.894642] (!!) init: process 'dhcpcd_wlan0', pid 3805 exited

<5>[  649.088015] (!!) init: starting 'dhcpcd_wlan0'

<4>[  651.788697] TouchPanel receive response in 5s, jiffies: 35060.

<1>[  652.942600] Unable to handle kernel NULL pointer dereference at virtual address 00000000

<1>[  652.951159] pgd = ab7c8000

<1>[  652.953913] [00000000] *pgd=3b5f6831, *pte=00000000, *ppte=00000000

<0>[  652.960788] Internal error: Oops: 17 [#1] PREEMPT SMP

<4>[  652.965845] Modules linked in: snd_usb_audio snd_usbmidi_lib snd_soc_imx_saf7741 mxc_asrc snd_soc_imx_mx2 snd_soc_imx_esai snd_soc_imx_ssi snd_soc_saf7741 snd_soc_core snd_aloop snd_rawmidi snd_hwdep asix cdc_ncm hdmi_mn864779 usbnet hid_ipod spi_ak7756 unifi_sdio snd_pcm snd_page_alloc snd_timer snd soundcore hid gp2ap050a virtual_ts atmel_mxt540e_ts uinput nls_utf8 nls_ascii autofs4 ch softdog pdrd galcore loop usb_storage ext4 jbd2 mbcache

<4>[  653.005594] CPU: 0    Not tainted  (3.0.35 #1)

<4>[  653.010062] PC is at put_page+0x0/0x40

<4>[  653.013826] LR is at skb_release_data+0x84/0xb4

<4>[  653.018364] pc : [<800bb388>]    lr : [<802a0bec>]    psr: 20000013

<4>[  653.018370] sp : ab6a7cf8  ip : 00000000  fp : 0000000c

<4>[  653.029859] r10: aa0feb00  r9 : ab6a7e18  r8 : a0b247c0

<4>[  653.035088] r7 : 00000000  r6 : a0b2464c  r5 : aa0feb00  r4 : 00000001

<4>[  653.041619] r3 : 00000006  r2 : 00000000  r1 : 00000000  r0 : 00000000

<4>[  653.048153] Flags: nzCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user

<4>[  653.055294] Control: 10c53c7d  Table: 3b7c804a  DAC: 00000015

<4>[  653.061043]

<4>[  653.061045] PC: 0x800bb308:

<4>[  653.065326] b308  ebffff52 e3a03000 e5843000 e28dd00c e8bd8ff0 e1a02001 e30a1adc e348100b

<4>[  653.073619] b328  eaffffc8 e52de004 e24dd00c e28d2008 e3a03000 e30a18b4 e348100b e5223004

<4>[  653.081911] b348  ebffffc0 e1a0200d e3c23d7f e3012cd0 e3c3303f e3482049 e5931014 e59f3018

<4>[  653.090205] b368  e7922101 e59d1004 e7930002 e0801001 e7831002 e28dd00c e8bd8000 8002eb54

<4>[  653.098498] b388  e5902000 e3120903 1a00000b e1a02000 e5b21004 f57ff05f e1921f9f e2411001

<4>[  653.106791] b3a8  e182cf91 e33c0000 1afffffa f57ff05f e3510000 112fff1e eafffead eafffeb6

<4>[  653.115086] b3c8  e92d4070 e1a04000 e5903000 e1500003 08bd8070 e3a06c01 e3a05c02 e3406010

<4>[  653.123379] b3e8  e3405020 e5943004 e2430018 e8930006 e5812004 e5821000 e5836000 e5835004

<4>[  653.131672]

<4>[  653.131674] LR: 0x802a0b6c:

<4>[  653.135955] 0b6c  e1a05000 e5d03064 e2032002 e6ef2072 e3520000 0a00000f e2033010 e3a02001

<4>[  653.144249] 0b8c  e6ef3073 e3530000 e5903094 17df2812 e2831028 f57ff05f e1910f9f e0400002

<4>[  653.152540] 0bac  e181cf90 e33c0000 1afffffa f57ff05f e3500000 18bd8038 e5950094 e1d030b0

<4>[  653.160832] 0bcc  e3530000 0a000009 da000008 e3a04000 e2843006 e2844001 e7900183 ebf869e6

<4>[  653.169125] 0bec  e5950094 e1d030b0 e1530004 cafffff7 e5903010 e3530000 0a000001 e2800010

<4>[  653.177417] 0c0c  ebffffca e5950098 e8bd4038 eaf8f789 e92d47f0 e2515000 e1a04000 e1a08003

<4>[  653.185709] 0c2c  e5903094 e5900098 ba000091 e594c0a4 e35c0001 1a00008b e5d41064 e0606003

<4>[  653.194002] 0c4c  e0866005 e201e002 e0866002 e286601f e6efe07e e3c6601f e35e0000 1a00005d

<4>[  653.202295]

<4>[  653.202297] SP: 0xab6a7c78:

<4>[  653.206577] 7c78  80072b9c a0b208bc 800f2cb8 00000000 a0b208c8 00000001 000000c3 00000001

<4>[  653.214870] 7c98  ab6a7cec 0000040f 00000007 a0b2464c 00000000 80035a90 00000000 00000000

<4>[  653.223163] 7cb8  00000000 00000006 00000001 aa0feb00 a0b2464c 00000000 a0b247c0 ab6a7e18

<4>[  653.231454] 7cd8  aa0feb00 0000000c 00000000 ab6a7cf8 802a0bec 800bb388 20000013 ffffffff

<4>[  653.239746] 7cf8  00000000 aa0feb00 ab6a6000 802a0934 a0b24600 80316908 00000001 8029c2e4

<4>[  653.248039] 7d18  a0b24800 00000ffc 00000000 00000001 ab6a7f74 0000000c a0b24794 00000000

<4>[  653.256330] 7d38  a0b2464c a84052c0 000007d1 aa5bc7a0 aa1a31e0 00000000 000009b2 00000000

<4>[  653.264622] 7d58  00000000 80382e34 aadab8a0 00000000 00000000 00000000 ab6a7ee0 00000ffc

<4>[  653.272916]

<4>[  653.272918] R5: 0xaa0fea80:

<4>[  653.277199] ea80  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

<4>[  653.285493] eaa0  00000000 00000000 8029d3b8 00000000 00000000 00000000 00000000 00000000

<4>[  653.293787] eac0  00000000 00000000 00000000 00000000 a0dc9dc0 a0dc9de0 a0dc9dc0 a0dc9dc0

<4>[  653.302080] eae0  000000c8 00000001 7a237e10 96aafeb6 154d5d1f a5e5d1fb 325634df f7affbf9

<4>[  653.310372] eb00  00000000 00000000 00000000 00000000 a0b24800 00000000 aa5bc7a0 aa1a31e0

<4>[  653.318663] eb20  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

<4>[  653.326956] eb40  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

<4>[  653.335248] eb60  00000000 00000000 80316640 00000000 00000000 00000000 00000000 00000000

<4>[  653.343541]

<4>[  653.343544] R6: 0xa0b245cc:

<4>[  653.347825] 45cc  00000000 00000000 00000000 00000000 00000000 00000000 00000000 a0b245e8

<4>[  653.356118] 45ec  a0b245e8 00000000 00000000 00000000 00000000 00000000 00000000 00000000

<4>[  653.364410] 460c  00010001 00000000 00000000 00000000 804b476c a0b24820 a0b24220 ffffffff

<4>[  653.372703] 462c  00000003 00000000 00000000 00000000 00000000 00000000 a0b24644 a0b24644

<4>[  653.380994] 464c  a0b2464c a0b2464c 00000000 00000000 00000000 00000000 00000000 00000000

<4>[  653.389287] 466c  00000000 00000000 00000000 00000000 0001a800 00000000 a0b208a0 00000000

<4>[  653.397582] 468c  00000000 00000100 00000000 00000000 00000000 00000001 00000000 0001a800

<4>[  653.405877] 46ac  a0b246ac a0b246ac 00000000 00000000 00000000 00010000 00000000 000000d0

<4>[  653.414171]

<4>[  653.414173] R8: 0xa0b24740:

<4>[  653.418454] 4740  ffffffff 00000000 c4653600 ffffffff a84052c0 00000000 00000000 00000000

<4>[  653.426747] 4760  00000000 00000000 00000000 00000000 8029c1dc 8029c2a8 80315c90 8029c178

<4>[  653.435039] 4780  00000000 80315b90 ab8f8be0 a82375e0 aa0231c0 00000000 00000000 00000000

<4>[  653.443330] 47a0  a0b247a0 a0b247a0 aadab8a0 a0b24800 00000000 a0b247b4 a0b247b4 00000000

<4>[  653.451624] 47c0  00000000 00000000 00000100 00000000 00000000

<3>[  653.456914] i2c i2c-3: <i2c_imx_trx_complete> I2C Control I2SR_IIF is Set, But I2C IRQ for GIC not trigger in HZ/2 Time

<3>[  653.456941] i2c i2c-2: <i2c_imx_trx_complete> I2C Control I2SR_IIF is Set, But I2C IRQ for GIC not trigger in HZ/2 Time

<4>[  653.479085]  00000000 00000000 00000000

<4>[  653.482958] 47e0  00000000 00000000 a0b247e8 a0b247e8 00000000 00000000 00000000 00000000

<4>[  653.491249] 4800  00000000 00000000 00000000 00010001 00000000 00000000 00000000 804b476c

<4>[  653.499540] 4820  a0566620 a0b24620 ffffffff 00000003 00000000 00000000 00000000 00000000

<4>[  653.507834]

<4>[  653.507836] R9: 0xab6a7d98:

<4>[  653.512117] 7d98  40000040 00000000 aadab8a0 ab6a6000 00000000 00000001 ffffffff 00000000

<4>[  653.520410] 7db8  00000000 00000000 00000000 00000000 aadab8a0 00000000 00000000 00000000

<4>[  653.528701] 7dd8  00000600 60000013 ab6a7e18 00000000 ab6a6000 80491cd0 ab6a6000 00020200

<4>[  653.536993] 7df8  00000000 00000024 a84052c0 00000000 00000000 ab6a7f74 00000018 ab6a7f74

<4>[  653.545285] 7e18  ab6a7e60 00000001 40000040 00000ffc a84052c0 00000000 ab6a7d44 ab6a7f74

<4>[  653.553578] 7e38  ab6a6000 ab6a7f74 ab6a7e80 00000002 40000040 ab6a7f00 00000010 00000000

<4>[  653.561870] 7e58  ab6a7f00 ab6a7f74 7eefa434 00000000 a84052c0 40000040 ab6a7f00 80299fe4

<4>[  653.570162] 7e78  00000000 7eefa460 a1ad7d88 800cb3f0 804b6480 804b6480 a1ad7d88 a1abfe84

<4>[  653.578456]

<4>[  653.578458] R10: 0xaa0fea80:

<4>[  653.582826] ea80  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

<4>[  653.591117] eaa0  00000000 00000000 8029d3b8 00000000 00000000 00000000 00000000 00000000

<4>[  653.599409] eac0  00000000 00000000 00000000 00000000 a0dc9dc0 a0dc9de0 a0dc9dc0 a0dc9dc0

<4>[  653.607702] eae0  000000c8 00000001 7a237e10 96aafeb6 154d5d1f a5e5d1fb 325634df f7affbf9

<4>[  653.615993] eb00  00000000 00000000 00000000 00000000 a0b24800 00000000 aa5bc7a0 aa1a31e0

<4>[  653.624284] eb20  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

<4>[  653.632576] eb40  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

<4>[  653.640867] eb60  00000000 00000000 80316640 00000000 00000000 00000000 00000000 00000000

<0>[  653.649163] Process wliautoserver (pid: 2001, stack limit = 0xab6a62f0)

<0>[  653.655782] Stack: (0xab6a7cf8 to 0xab6a8000)

<0>[  653.660144] 7ce0:                                                       00000000 aa0feb00

<0>[  653.668332] 7d00: ab6a6000 802a0934 a0b24600 80316908 00000001 8029c2e4 a0b24800 00000ffc

<0>[  653.676519] 7d20: 00000000 00000001 ab6a7f74 0000000c a0b24794 00000000 a0b2464c a84052c0

<0>[  653.684705] 7d40: 000007d1 aa5bc7a0 aa1a31e0 00000000 000009b2 00000000 00000000 80382e34

<0>[  653.692893] 7d60: aadab8a0 00000000 00000000 00000000 ab6a7ee0 00000ffc ab6a7f74 40000040

<0>[  653.701080] 7d80: 80382e34 00000000 00000000 ab6a7f00 00000010 802992dc 40000040 00000000

<0>[  653.709266] 7da0: aadab8a0 ab6a6000 00000000 00000001 ffffffff 00000000 00000000 00000000

<0>[  653.717451] 7dc0: 00000000 00000000 aadab8a0 00000000 00000000 00000000 00000600 60000013

<0>[  653.725637] 7de0: ab6a7e18 00000000 ab6a6000 80491cd0 ab6a6000 00020200 00000000 00000024

<0>[  653.733822] 7e00: a84052c0 00000000 00000000 ab6a7f74 00000018 ab6a7f74 ab6a7e60 00000001

<0>[  653.742008] 7e20: 40000040 00000ffc a84052c0 00000000 ab6a7d44 ab6a7f74 ab6a6000 ab6a7f74

<0>[  653.750193] 7e40: ab6a7e80 00000002 40000040 ab6a7f00 00000010 00000000 ab6a7f00 ab6a7f74

<0>[  653.758379] 7e60: 7eefa434 00000000 a84052c0 40000040 ab6a7f00 80299fe4 00000000 7eefa460

<0>[  653.766565] 7e80: a1ad7d88 800cb3f0 804b6480 804b6480 a1ad7d88 a1abfe84 a1abfe74 800ce680

<0>[  653.774750] 7ea0: 84437620 84437640 00000001 00000000 00000001 800b6e64 00000000 84437620

<0>[  653.782936] 7ec0: 00000000 84437620 ab5ea7a0 802989a4 80298988 80116e4c ab5ea7a0 ab5ea7e0

<0>[  653.791122] 7ee0: 0006c668 ab5ea7a0 ab5ea7e0 ab6a7f08 ab5ea7a8 80116de4 ffffffff ab5ea7a0

<0>[  653.799307] 7f00: 0006c0fc 00000224 0006b320 00000dcc 00000020 ab6a6000 7eefa568 aa256680

<0>[  653.807493] 7f20: ab5ea7a0 ffffffff 00000001 801181b4 00000000 a1ad7d88 00000000 800e4698

<0>[  653.815678] 7f40: fffffff7 a84052c0 40000040 7eefa434 00000129 80036244 ab6a6000 00000000

<0>[  653.823864] 7f60: 00000000 8029b310 00000000 7eefa558 2ae50ea0 00000000 00000000 ab6a7f00

<0>[  653.832049] 7f80: 00000002 7eefa460 0000007c 40000000 00000001 fffffff7 7eefa434 00000040

<0>[  653.840235] 7fa0: 0000006a 800360c0 7eefa434 00000040 0000006a 7eefa434 40000040 00000000

<0>[  653.848420] 7fc0: 7eefa434 00000040 0000006a 00000129 7eefa568 2aad7f10 2aad7f10 00000000

<0>[  653.856606] 7fe0: 00000000 7eefa410 2aafebb4 2aafebc4 80000010 0000006a e1d330fe e5900000

<4>[  653.864817] [<800bb388>] (put_page+0x0/0x40) from [<802a0bec>] (skb_release_data+0x84/0xb4)

<4>[  653.873186] [<802a0bec>] (skb_release_data+0x84/0xb4) from [<802a0934>] (__kfree_skb+0x14/0xcc)

<4>[  653.881903] [<802a0934>] (__kfree_skb+0x14/0xcc) from [<80316908>] (unix_stream_recvmsg+0x218/0x64c)

<4>[  653.891050] [<80316908>] (unix_stream_recvmsg+0x218/0x64c) from [<802992dc>] (sock_recvmsg+0xa0/0xc0)

<4>[  653.900282] [<802992dc>] (sock_recvmsg+0xa0/0xc0) from [<80299fe4>] (__sys_recvmsg+0xfc/0x1b4)

<4>[  653.908905] [<80299fe4>] (__sys_recvmsg+0xfc/0x1b4) from [<8029b310>] (sys_recvmsg+0x3c/0x68)

<4>[  653.917447] [<8029b310>] (sys_recvmsg+0x3c/0x68) from [<800360c0>] (ret_fast_syscall+0x0/0x30)

<0>[  653.926070] Code: e7831002 e28dd00c e8bd8000 8002eb54 (e5902000)

<4>[  653.935272] ---[ end trace ea32b4c44717477d ]---

<0>[  653.940265] Kernel panic - not syncing: Fatal exception

<4>[  653.945630] [<8003cd9c>] (unwind_backtrace+0x0/0xf8) from [<8035a938>] (panic+0x74/0x18c)

<4>[  653.953934] [<8035a938>] (panic+0x74/0x18c) from [<80039bb4>] (die+0x218/0x284)

<4>[  653.961345] [<80039bb4>] (die+0x218/0x284) from [<8035a730>] (__do_kernel_fault.part.5+0x54/0x74)

<4>[  653.970298] [<8035a730>] (__do_kernel_fault.part.5+0x54/0x74) from [<800409c4>] (do_page_fault+0x2b4/0x31c)

<4>[  653.980117] [<800409c4>] (do_page_fault+0x2b4/0x31c) from [<80030410>] (do_DataAbort+0x34/0x9c)

<4>[  653.988895] [<80030410>] (do_DataAbort+0x34/0x9c) from [<80035a90>] (__dabt_svc+0x70/0xa0)

<4>[  653.997207] Exception stack(0xab6a7cb0 to 0xab6a7cf8)

<4>[  654.002280] 7ca0:                                     00000000 00000000 00000000 00000006

<4>[  654.010497] 7cc0: 00000001 aa0feb00 a0b2464c 00000000 a0b247c0 ab6a7e18 aa0feb00 0000000c

<4>[  654.018735] 7ce0: 00000000 ab6a7cf8 802a0bec 800bb388 20000013 ffffffff

<4>[  654.025421] [<80035a90>] (__dabt_svc+0x70/0xa0) from [<800bb388>] (put_page+0x0/0x40)

<4>[  654.033313] [<800bb388>] (put_page+0x0/0x40) from [<802a0bec>] (skb_release_data+0x84/0xb4)

<4>[  654.041740] [<802a0bec>] (skb_release_data+0x84/0xb4) from [<802a0934>] (__kfree_skb+0x14/0xcc)

<4>[  654.050495] [<802a0934>] (__kfree_skb+0x14/0xcc) from [<80316908>] (unix_stream_recvmsg+0x218/0x64c)

<4>[  654.059674] [<80316908>] (unix_stream_recvmsg+0x218/0x64c) from [<802992dc>] (sock_recvmsg+0xa0/0xc0)

<4>[  654.068945] [<802992dc>] (sock_recvmsg+0xa0/0xc0) from [<80299fe4>] (__sys_recvmsg+0xfc/0x1b4)

<4>[  654.077606] [<80299fe4>] (__sys_recvmsg+0xfc/0x1b4) from [<8029b310>] (sys_recvmsg+0x3c/0x68)

<4>[  654.086163] [<8029b310>] (sys_recvmsg+0x3c/0x68) from [<800360c0>] (ret_fast_syscall+0x0/0x30)

<2>[  654.094827] CPU1: stopping

<4>[  654.097569] [<8003cd9c>] (unwind_backtrace+0x0/0xf8) from [<800303a8>] (do_IPI+0x1d4/0x208)

<4>[  654.105935] [<800303a8>] (do_IPI+0x1d4/0x208) from [<80035b0c>] (__irq_svc+0x4c/0xe8)

<4>[  654.113771] Exception stack(0xa1ae7eb0 to 0xa1ae7ef8)

<4>[  654.118829] 7ea0:                                     8480ff20 aab54b20 047e1000 00000000

<4>[  654.127015] 7ec0: 8480ff20 a1a3a460 a1ae6000 aab54b20 a1a3a5e8 a1ae6000 7ebf0e50 a1ae7fac

<4>[  654.135200] 7ee0: aab54b20 a1ae7ef8 8035dc74 8035fee0 60000113 ffffffff

<4>[  654.141832] [<80035b0c>] (__irq_svc+0x4c/0xe8) from [<8035fee0>] (_raw_spin_unlock_irq+0x18/0x40)

<4>[  654.150716] [<8035fee0>] (_raw_spin_unlock_irq+0x18/0x40) from [<8035dc74>] (__schedule+0x198/0x6d8)

<4>[  654.159861] [<8035dc74>] (__schedule+0x198/0x6d8) from [<80036120>] (ret_slow_syscall+0x0/0x4)

.

Best

Labels (1)
Tags (2)
1 Solution
3,004 Views
jianxingwang
Contributor II

Hi

Thank you for your response.

The issue is caused by refree the SKB buffer by wifi driver, and has been fixed.

Best

Jianxing Wang

View solution in original post

0 Kudos
Reply
3 Replies
3,004 Views
igorpadykov
NXP Employee
NXP Employee

Hi jianxing

probably you used wrong csr driver, recommended

to apply to csr and request updated driver for your specific wifi module.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

3,005 Views
jianxingwang
Contributor II

Hi

Thank you for your response.

The issue is caused by refree the SKB buffer by wifi driver, and has been fixed.

Best

Jianxing Wang

0 Kudos
Reply
3,004 Views
jianxingwang
Contributor II

Thank you for your response.

Could please help me to analysis the possibility reason that can caused this panic?

Best

Jianxing Wang

0 Kudos
Reply