iMX6DL Booting from Nand

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX6DL Booting from Nand

跳至解决方案
1,438 次查看
JackLEE_
Contributor II

Hi community,

I am working on custom board based on i.MX6DL sabreSD.

I have success with boot from SD card and now I want to boot from Nand flash(MX30LF4G18AC).

However, after burning the image to Nand, i get the error "ubi_io_read: error -74 (ECC error) while reading 126976 bytes from PEB 4:4096, read 126976 bytes" which can be seen in first boot log. Then, I reboot the board (second boot log), it just jump into kernel panic.

 

How to fix this error?

Any advice would be grateful.

 

 

标签 (3)
标记 (2)
0 项奖励
回复
1 解答
1,410 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

The error -74 is related to the issue filed in MTD (Memory Technology Devices).

Please check the following link and verify if you used the ubiformat to flash the image to NAND, you need to enable the “-space-fixeup”

Best regards.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,411 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

The error -74 is related to the issue filed in MTD (Memory Technology Devices).

Please check the following link and verify if you used the ubiformat to flash the image to NAND, you need to enable the “-space-fixeup”

Best regards.

0 项奖励
回复