iMX6 ul Boot mode question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX6 ul Boot mode question

跳至解决方案
1,541 次查看
chrisszot
Contributor I

I am using a iMX6UL and I am trying to boot from eMMC connected to SDIO2.  I am using a lot of GPIO's and do not want to use all of the LCD_DATA lines just for the boot configuration. 

I have installed two testpoints on the BOOT_MODE pins to allow us to enter serial flash mode with a test fixture, then when we remove the board from our test bench we pull these lines low to enable boot from fuses.

I am trying to understand the fusing details to ensure this works.  There are recommendations which state to leave the LCD_DATA lines open, or use a bunch of analogue switches to enable after boot to not enter an incorrect boot mode.  Is this really necessary?  If we enter serial mode, is there any way to boot from internal fuses and not use the GPIOs?  Or is fusing even needed/ could we boot off internal, have that be a bootloader to point to eMMC and set up the system correctly?

0 项奖励
回复
1 解答
1,175 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Chris

after entering serial mode there no way to boot from internal fuses, as

processor will execute Serial Downloader commands, flow is described in

sect.8.9 Serial Downloader i.MX6UL Reference Manual (rev.1  4/2016)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf

Booting from fuses is described in sect.8.2.3 Boot From Fuses Mode

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,176 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Chris

after entering serial mode there no way to boot from internal fuses, as

processor will execute Serial Downloader commands, flow is described in

sect.8.9 Serial Downloader i.MX6UL Reference Manual (rev.1  4/2016)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf

Booting from fuses is described in sect.8.2.3 Boot From Fuses Mode

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复