iMX6 solo problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,045件の閲覧回数
wanglee
Contributor III

My mfgtools support  iMX6Q/iMX6D,  it works right.  but it didn't  support my iMX6 solo. when the power on, "No Device Connected".  I don't think this is a hardware problem.  what should I DO?   CHANGE the settings  of mfgtool ?~ZFILHAZJN4K56YS[]95U}Q.png

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,880件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   Please try using the recent MFG 

http://www.nxp.com/webapp/Download?colCode=IMX6_L4-1-15_2-0-0_MFG-TOOL&appType=license&location=null... 

 

  Also, please check if the i.MX6 S board is configured for serial (USB) boot mode ;

BOOT_MODE[1:0] = 01 (Serial Downloader).

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,881件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   Please try using the recent MFG 

http://www.nxp.com/webapp/Download?colCode=IMX6_L4-1-15_2-0-0_MFG-TOOL&appType=license&location=null... 

 

  Also, please check if the i.MX6 S board is configured for serial (USB) boot mode ;

BOOT_MODE[1:0] = 01 (Serial Downloader).

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

 

0 件の賞賛
返信
2,880件の閲覧回数
wanglee
Contributor III

NOW ,the new tool (mfgtools-without-rootfs) can  find  my  iMX6Q .  when power on ,it shows HID-compliant device. then  START,  it always get stuck  in here  what is the problem?

9D$U{($FHK{}(U]N%J2HNC8.png

0 件の賞賛
返信
2,880件の閲覧回数
wanglee
Contributor III

The recent MFG, it works.  thanks.

0 件の賞賛
返信