iMX6 linux development

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 linux development

3,054 Views
Chicago1984
Contributor II

I am having some development system startup issues with ltib on the i.MX6.  I have seen that some people use yocto, which also is giving me headaches.  I would rather work at a low level, with the kernel source code and a functional file system, I am having problems getting a cross-compiled app to work with the existing linux SD cards that we have. What other paths are developers using?

Labels (3)
3 Replies

2,760 Views
Yuri
NXP Employee
NXP Employee

The following may be helpful for Linux applications development.

"AN3870  Developing an Application for the i.MX Devices on Linux Platform"

http://cache.freescale.com/files/dsp/doc/app_note/AN3870.pdf

The next app note may be useful in debugging :

"AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors."

http://cache.freescale.com/files/32bit/doc/app_note/AN4553.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,760 Views
sinanakman
Senior Contributor III

Hi Shahzad, we simply use mainline Linux kernel and buildroot to build a simple root file system to test out things on our sabre SD board.

Hope this helps

Sinan Akman

2,760 Views
LeonardoSandova
Specialist I

Shahzad, your headaches are understandable :smileyhappy: Yocto is a completely different system but it is the way to go for integrating your packages/drivers. What are the specific problems you have? Are you using the cross-toolchain produced by bitbake?

0 Kudos
Reply