iMX6 kernel L3.0.35 build error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 kernel L3.0.35 build error

ソリューションへジャンプ
7,933件の閲覧回数
xiaoqiangyang
Contributor III

Now, I am using ltib building linux kernel for IMX6, but failed and got the message below:

......

......

LD vmlinux.o

  MODPOST vmlinux.o

  GEN.version
  CHKinclude/generated/compile.h
  UPDinclude/generated/compile.h
  CC init/version.o
  LD init/built-in.o
  LD .tmp_vmlinux1

arch/arm/mach-mx6/built-in.o: In function `pfuze100_init':

usb_h1.c:(.text+0xf9ac): undefined reference to `pfuze_reg_read'

usb_h1.c:(.text+0xf9d0): undefined reference to `pfuze_reg_read'

usb_h1.c:(.text+0xfa00): undefined reference to `pfuze_reg_write'

usb_h1.c:(.text+0xfa44): undefined reference to `pfuze_reg_rmw'

usb_h1.c:(.text+0xfa60): undefined reference to `pfuze_reg_rmw'

usb_h1.c:(.text+0xfa84): undefined reference to `pfuze_reg_rmw'

usb_h1.c:(.text+0xfaa0): undefined reference to `pfuze_reg_rmw'

usb_h1.c:(.text+0xfac8): undefined reference to `pfuze_reg_rmw'

arch/arm/mach-mx6/built-in.o:usb_h1.c:(.text+0xfae4): more undefined references to `pfuze_reg_rmw' follow

arch/arm/mach-mx6/built-in.o: In function `pfuze100_init':

usb_h1.c:(.text+0xfb5c): undefined reference to `pfuze_reg_write'

usb_h1.c:(.text+0x10594): undefined reference to `pfuze_reg_read'

usb_h1.c:(.text+0x105b8): undefined reference to `pfuze_reg_read'

usb_h1.c:(.text+0x105e8): undefined reference to `pfuze_reg_write'

usb_h1.c:(.text+0x1062c): undefined reference to `pfuze_reg_rmw'

usb_h1.c:(.text+0x10648): undefined reference to `pfuze_reg_rmw'

usb_h1.c:(.text+0x1066c): undefined reference to `pfuze_reg_rmw'

usb_h1.c:(.text+0x10688): undefined reference to `pfuze_reg_rmw'

usb_h1.c:(.text+0x106b0): undefined reference to `pfuze_reg_rmw'

arch/arm/mach-mx6/built-in.o:usb_h1.c:(.text+0x106cc): more undefined references to `pfuze_reg_rmw' follow

arch/arm/mach-mx6/built-in.o: In function `pfuze100_init':

usb_h1.c:(.text+0x10744): undefined reference to `pfuze_reg_write'

arch/arm/mach-mx6/built-in.o: In function `regulators_init':

usb_h1.c:(.init.text+0x8d8): undefined reference to `anatop_register_regulator'

usb_h1.c:(.init.text+0x8e8): undefined reference to `anatop_register_regulator'

usb_h1.c:(.init.text+0x8f8): undefined reference to `anatop_register_regulator'

usb_h1.c:(.init.text+0x908): undefined reference to `anatop_register_regulator'

usb_h1.c:(.init.text+0x918): undefined reference to `anatop_register_regulator'

arch/arm/mach-mx6/built-in.o:usb_h1.c:(.init.text+0x928): more undefined references to `anatop_register_regulator' follow

arch/arm/mach-mx6/built-in.o: In function `max17135_regulator_init':

usb_h1.c:(.init.text+0x15d8): undefined reference to `max17135_register_regulator'

arch/arm/mach-mx6/built-in.o: In function `mx6_sabresd_board_init':

usb_h1.c:(.init.text+0x1cac): undefined reference to `imx_add_imx_pxp'

usb_h1.c:(.init.text+0x1cb0): undefined reference to `imx_add_imx_pxp_client'

usb_h1.c:(.init.text+0x1cd8): undefined reference to `imx_add_imx_epdc'

usb_h1.c:(.init.text+0x1f48): undefined reference to `imx_add_perfmon'

usb_h1.c:(.init.text+0x1f50): undefined reference to `imx_add_perfmon'

usb_h1.c:(.init.text+0x1f60): undefined reference to `imx_add_perfmon'

usb_h1.c:(.init.text+0x20e8): undefined reference to `imx6dl_pxp_data'

usb_h1.c:(.init.text+0x20f4): undefined reference to `imx6dl_epdc_data'

usb_h1.c:(.init.text+0x213c): undefined reference to `imx6q_perfmon_data'

usb_h1.c:(.init.text+0x2140): undefined reference to `imx6q_perfmon_data'

usb_h1.c:(.init.text+0x2144): undefined reference to `imx6q_perfmon_data'

arch/arm/mach-mx6/built-in.o: In function `mx6_board_init':

usb_h1.c:(.init.text+0x2c3c): undefined reference to `imx_add_mlb'

usb_h1.c:(.init.text+0x2c78): undefined reference to `imx_add_perfmon'

usb_h1.c:(.init.text+0x2c80): undefined reference to `imx_add_perfmon'

usb_h1.c:(.init.text+0x2c90): undefined reference to `imx_add_perfmon'

usb_h1.c:(.init.text+0x2e7c): undefined reference to `imx6q_perfmon_data'

usb_h1.c:(.init.text+0x2e80): undefined reference to `imx6q_perfmon_data'

usb_h1.c:(.init.text+0x2e84): undefined reference to `imx6q_perfmon_data'

drivers/built-in.o: In function `mxc_hdmi_register_audio':

clkdev.c:(.text+0x54af4): undefined reference to `snd_pcm_link_rwlock'

drivers/built-in.o: In function `mxc_hdmi_abort_stream':

clkdev.c:(.text+0x54bac): undefined reference to `snd_pcm_link_rwlock'

drivers/built-in.o: In function `asrc_init':

clkdev.c:(.init.text+0x5c1c): undefined reference to `asrc_p2p_hook'

drivers/built-in.o: In function `asrc_exit':

clkdev.c:(.exit.text+0xa80): undefined reference to `asrc_p2p_hook'

make: *** [.tmp_vmlinux1] Error 1

error: Bad exit status from /home/yxq/iMX6/L3.0.35_4.0.0_130424_source/ltib/tmp/rpm-tmp.34384 (%build)

RPM build errors:

Bad exit status from /home/yxq/iMX6/L3.0.35_4.0.0_130424_source/ltib/tmp/rpm-tmp.34384 (%build)

Build time for kernel-3.0.35: 679 seconds

Failed building kernel-3.0.35

f_buildrpms() returned an error, exiting

traceback:

main:572

Started: Mon Dec  9 11:05:12 2013

Ended:   Mon Dec  9 11:16:32 2013

Elapsed: 680 seconds

These packages failed to build:

kernel-3.0.35

Build Failed

So many undefined references, I tried many times but failed. Any one knows the solution?

Thanks in advance!

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
3,424件の閲覧回数
lily_zhang
NXP Employee
NXP Employee

Did you run "distclean"  to clean up old objects? Meanwhile, check which defconfig file you are using.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,424件の閲覧回数
Raybiztech
Contributor V

Hi Xiaoqiang,

I Think you have disabled CONFIG_MFD_PFUZE. You can enable it and check once. You can find this option in device driver ->Multifunction device drivers->Support for Freescale's PMIC PFUZE. This will also work. Also using default config for imx6 enables this option by default.

Thanks and Regards,

RayBizTech.

0 件の賞賛
返信
3,424件の閲覧回数
xiaoqiangyang
Contributor III

Hi Raybiztech,

I tried your method and succeeded. Thanks for your advice, it's very useful to me!

0 件の賞賛
返信
3,425件の閲覧回数
lily_zhang
NXP Employee
NXP Employee

Did you run "distclean"  to clean up old objects? Meanwhile, check which defconfig file you are using.

0 件の賞賛
返信
3,424件の閲覧回数
xiaoqiangyang
Contributor III

Thanks,Xiaoli,I run 'distclean' and the problem has been solved!

0 件の賞賛
返信