iMX6: how to trigger software reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6: how to trigger software reset

50,913 Views
rafalwegner
Contributor II

Hello

Does anyone knows and could describe the procedure of how to trigger a reset of the board (power off / power on) from software (u-boot application)?

I believe some of the SRC registers should be configured properly to obtain such behaviour.

Thanks very much in advance

BR, Rafal

Labels (1)
30 Replies

12,148 Views
zlhuang
Contributor I

Thanks, Yongcai.

Do you mean it's the hardware circuit issue?

I will monitor the POR pin and report the result.

0 Kudos
Reply

6,736 Views
rafalwegner
Contributor II

Hello

Thanks for your answer but what I actually would like to do is to reset the i.MX6 SOC from standalone program run in u-boot. From within this standalone program I would like to have the same behaviour (reset of iMX6) as user can trigger by running "reset" command in u-boot prompt.

Do you know how to trigger a wdog reset using internal iMX6 registers? Those settings of registers are what I am looking for.

BR, Rafal

0 Kudos
Reply

6,736 Views
AnsonHuang
NXP Employee
NXP Employee

Hi,Rafal

       Sorry for taking your question in wrong way, below are the answers:

        To trigger wdog reset, you can write 0x4 to wdog's control register, it's address should be 0x21bc000, it is a 16 bits register, you need to write it in 16 bits access.

         For SRC register, bit 0 of SRC_SCR register is to control whether you want a warm reset of cold reset of system. It's address should be 0x20d8000.

          Please try it and let me know the result, thanks.

6,737 Views
mrleo
Contributor IV

Dear Yongcai,


Since my board hardware problem, I need to a warm reset my board  with the WDOG1, like uboot "reset", only reset POR.

freescale code default support WDOG2,a cold reset.Third-party kernel like openwrt imx6q kernel support warm reset.

I modify some code below:

1.arch/arm/mach-mx6/cpu.c

/* Disable SRC warm reset to work aound system reboot issue */

  base = IO_ADDRESS(SRC_BASE_ADDR);

  reg = __raw_readl(base);

  //reg &= ~0x1;

  reg |=0x1;//force SRC warm reset  add 20140421

  __raw_writel(reg, base);

2.arch/arm/plat-mxc/system.c

//add

#define SRC_SCR 0x000

#define SRC_GPR1 0x020

#define BP_SRC_SCR_WARM_RESET_ENABLE 0

#define BP_SRC_SCR_CORE1_RST 14

#define BP_SRC_SCR_CORE1_ENABLE 22

void imx_src_prepare_restart(void)

{

  u16 val;

  /* clear enable bits of secondary cores */

  val = __raw_readw(IO_ADDRESS(0x20d8000));//src_scr

  val &= ~(0x7<< BP_SRC_SCR_CORE1_ENABLE);

  printk("SRC_SCR=0x%x\n",val);//val=521

  //__raw_writew(0,IO_ADDRESS(0x20bc008));//WDOG_WMCR diable counter optertion

  /* clear persistent entry register of primary core */

  __raw_writew(0,IO_ADDRESS(0x20d8020));//src_gpr1 core1

  __raw_writew(0,IO_ADDRESS(0x20d8024));

  __raw_writew(0,IO_ADDRESS(0x20d8028));//core2

  __raw_writew(0,IO_ADDRESS(0x20d802c));

  __raw_writew(0,IO_ADDRESS(0x20d8030));

  __raw_writew(0,IO_ADDRESS(0x20d8034));//core3

  __raw_writew(0,IO_ADDRESS(0x20d8038));

  __raw_writew(0,IO_ADDRESS(0x20d803c));//core4

}

void arch_reset(char mode, const char *cmd)

{

  unsigned int wcr_enable;

  printk("%s\n",__FILE__);

  arch_reset_special_mode(mode, cmd);

  imx_src_prepare_restart();

#ifdef CONFIG_ARCH_MX6

#if 0

  /* wait for reset to assert... */

  if (enable_ldo_mode == LDO_MODE_BYPASSED) {

  /*On Sabresd board use WDOG2 to reset external PMIC, so here do

  * more WDOG2 reset.*/

  printk("WDOG2\n");

  wcr_enable = 0x14;

  __raw_writew(wcr_enable, IO_ADDRESS(MX6Q_WDOG2_BASE_ADDR));

  __raw_writew(wcr_enable, IO_ADDRESS(MX6Q_WDOG2_BASE_ADDR));

  } else

#endif

  wcr_enable = 0x4;

  __raw_writew(wcr_enable, wdog_base);

  /* errata TKT039676, SRS bit may be missed when

  SRC sample it, need to write the wdog controller

  twice to avoid it */

  __raw_writew(wcr_enable, wdog_base);

  /* wait for reset to assert... */

  mdelay(500);

  printk(KERN_ERR "Watchdog reset failed to assert reset\n");

  mdelay(500);

  return;

#endif

}

But also not reboot the system? imx6q linux 3.0.35 can support software warm reset or not?

If can,what should I do?

0 Kudos
Reply

6,737 Views
AnsonHuang
NXP Employee
NXP Employee

We do NOT support warm reset in our BSP, if you want to use warm reset, LDO bypass will be not supported, and MMDC auto self-refresh must be disabled.

May I know why you want to use WARM reset? COLD reset is OK for you, I thought you just NOT want the WDOG to trigger external PMIC reset, then code reset should be OK for you, right?

0 Kudos
Reply

6,737 Views
mrleo
Contributor IV

Dear Yongcai,


I am very sorry ,Because of my board hardware problem,cold reset in not ok for me , I need to a warm reset my board  with the WDOG1,like in uboot reset.

if i want to use warm reset, how to disable LDO bypass , and MMDC auto self-refresh.


Thanks


Leo

0 Kudos
Reply

6,737 Views
AnsonHuang
NXP Employee
NXP Employee

uboot reset can also be colde reset, we have three kinds of reset, you can refer to RM for detail, I think cold reset is OK for you, you just don't want a power reset, right? To disable LDO bypass, for L3.0.35, you can add "ldo_active=on" to kernel command line, after kernel boot up, you can measure the VDDARM_IN, it should be 1.375V for 1GHz part. Then no need to disable MMDC auto self-refresh if using cold reset.

0 Kudos
Reply

6,737 Views
mrleo
Contributor IV

Thanks very much!It is ok for me!

0 Kudos
Reply

6,737 Views
AnsonHuang
NXP Employee
NXP Employee

Great, I am glad to hear that:)

0 Kudos
Reply

6,737 Views
rafalwegner
Contributor II

Hi

Thanks very much for your input. I am working on iMX6 DualLite processor and to trigger wdog reset I had to clear fourth bit of WDOG1_WCR register (0x020bc000). Now my program works as I needed.

Best Regards

Rafal

0 Kudos
Reply