iMX6 display rotation example fail at resolution 1280x800

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6 display rotation example fail at resolution 1280x800

2,059 次查看
ivanpankratov
Contributor II

Hello,

I am trying to run a rotation example from here: GitHub - rogeriorps/ipu-examples: IPU example codes for i.MX5 and i.MX6 families 

My display resolution is 1280x800. When I take the same size input image the provided example able to perform all flips but not to rotate:

isize value 2048000

Rotation 0 time: 4741 usecs
Rotation 1 time: 4589 usecs
Rotation 2 time: 4554 usecs
Rotation 3 time: 4615 usecs
[19493.497581] mxc_ipu mxc_ipu: ERR: no-0x0,ipu_queue_task err:-22
ioct IPU_QUEUE_TASK fail

If I take 1024x768 input image and 1280x800 output resolution -- the same result.

But if I take 1024x768 input and output resolutions, all possible 8 flips and rotations work, though I observe an interlaced garbage on my screen, due to wrong output resolution:

isize value 1572864
Rotation 0 time: 6144 usecs
Rotation 1 time: 6166 usecs
Rotation 2 time: 6152 usecs
Rotation 3 time: 6152 usecs
Rotation 4 time: 29750 usecs
Rotation 5 time: 21677 usecs
Rotation 6 time: 21586 usecs
Rotation 7 time: 21605 usecs

I understand that this is related to IPU's rotator limitation of 1024x1024 pixel size, but still, how to make all rotations work? I am running it on kernel 4.1.15.

Thanks, Ivan

标记 (2)
0 项奖励
回复
2 回复数

1,498 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ivan

IPU does not support rotation (limitation of IC module) above 1024x1024,
so one needs to split image on smaller areas and rotate them, after that combine
to whole image. Please check for example below

https://community.freescale.com/message/567360#567360

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,498 次查看
ivanpankratov
Contributor II

Thanks Igor, will take a look.

Don't you have it implemented as a fb driver?

0 项奖励
回复