iMX6 devices without CAAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 devices without CAAM

Jump to solution
3,774 Views
mtrx
Contributor I

Hi, in AN12714 about Encrypted Storage using CAAM is stated: "The document applies to all i.MX SoCs having CAAM module. The feature is not available on i.MX SoCs with DCP." I searched through several product data sheets but cannot find a clear reference about "DCP" and which iMX SoCs actually do not support CAAM. Can someone help on this? Thanks, Michael

0 Kudos
Reply
1 Solution
3,759 Views
joanxie
NXP TechSupport
NXP TechSupport

you can refer to the enclosed file, imx6ull has DCP but no CAAM which is like imx6sl, i.mx6ul doesn't support DCP

View solution in original post

2 Replies
3,760 Views
joanxie
NXP TechSupport
NXP TechSupport

you can refer to the enclosed file, imx6ull has DCP but no CAAM which is like imx6sl, i.mx6ul doesn't support DCP

3,767 Views
mihai_chelalau
NXP Employee
NXP Employee

Hi, Michael

I will discuss this with my other teammates which are more familiar with the 6 Series and come back with an answer ASAP. 

Kind regards, 

MC

0 Kudos
Reply