iMX6 devices without CAAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 devices without CAAM

ソリューションへジャンプ
3,710件の閲覧回数
mtrx
Contributor I

Hi, in AN12714 about Encrypted Storage using CAAM is stated: "The document applies to all i.MX SoCs having CAAM module. The feature is not available on i.MX SoCs with DCP." I searched through several product data sheets but cannot find a clear reference about "DCP" and which iMX SoCs actually do not support CAAM. Can someone help on this? Thanks, Michael

0 件の賞賛
返信
1 解決策
3,695件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

you can refer to the enclosed file, imx6ull has DCP but no CAAM which is like imx6sl, i.mx6ul doesn't support DCP

元の投稿で解決策を見る

2 返答(返信)
3,696件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

you can refer to the enclosed file, imx6ull has DCP but no CAAM which is like imx6sl, i.mx6ul doesn't support DCP

3,703件の閲覧回数
mihai_chelalau
NXP Employee
NXP Employee

Hi, Michael

I will discuss this with my other teammates which are more familiar with the 6 Series and come back with an answer ASAP. 

Kind regards, 

MC

0 件の賞賛
返信