iMX6 booting problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 booting problems

2,193件の閲覧回数
pieter
Contributor II

Hi community,

I have problems with booting my iMX6 board.


It doesn't start u-boot and goes automatically into recovery mode.

Any idea's?

ラベル(1)
0 件の賞賛
返信
1 返信

1,552件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please check Your design, using recommendations  of Chapter 8 (Avoiding Board Bring-up
Problems) of “Hardware Development Guide for i.MX 6Quad,6Dual, 6DualLite, 6Solo Families …”

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

  Also You may use the next "HW Design Checklist for i.MX6" to check the schematic themselves :

https://community.freescale.com/docs/DOC-93819

Do You have enough memory ?

Is memory configuration correct ?

What are bootargs ?


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信