Hy,
I am doing a design around iMX6 ULZ processor and have downloaded the reference design files from here . I have converted the gerber files to altium pcb file and copied the DRAM traces to my design.
In Altium I have rules set up for matching lengths according to Hardware Development Guide for the i.MX 6ULL Application Processor , specifically the DDR3 routing by byte group as in table below:

But some of the groups from your reference design are not matched to this spec. For examle:
DATA HIGH group is matched within this spec. All signals, including SDQS1 are around 27.1 mm
but
DATA LOW group has data signals lengthmatched to around 25mm but SDQS0 are matched to 30,6mm ... that is more than 4mm diffence, much more than 25mil (0.635mm) spec.
and even more strange are the Address signals
About half of those are 38mm and other half is 35mm

Now, only explanation would be the board thicknes and via lengths. Have you included the via lengths in your lengths, because 3-5 mm difference seems too much for ddr3. How thick is the board? It just seems strange