How to boot Linux directly from UUU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to boot Linux directly from UUU

Jump to solution
2,214 Views
Ryo_Aoki
Contributor III

Hi community.

I am currently using an i.MX6 SabreAI board.
I want to boot linux directly from serial downloader mode without writing to emmc or QSPI or SD card.
Is such usage possible?

 

I have already checked the following documents, but I do not understand the procedure.
whether it can be used in such a way
If possible, could you please tell me the command procedure?

 UUU (Universal Update Utility)Document (uuu.pdf)
 https://github.com/nxp-imx/mfgtools
 LF5.15.71.2.2.0のLinuxUserGuide

Labels (1)
0 Kudos
Reply
1 Solution
2,200 Views
joanxie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
2 Replies
2,201 Views
joanxie
NXP TechSupport
NXP TechSupport

i.mx6 can boot up from usb, you can refer to the old community link

"https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Booting-Linux-through-USB-on-the-i-MX6-s..."

 

0 Kudos
Reply
2,125 Views
Ryo_Aoki
Contributor III

thank you for your reply. I will check the docs and give it a try.

0 Kudos
Reply