iMX6 Sabre SD Hardware Debugger - Application level

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 Sabre SD Hardware Debugger - Application level

ソリューションへジャンプ
1,621件の閲覧回数
raz3l
Contributor III


Hi!

I was wondering if the DS-5 Debugger from ARM is capable of debugging at the application level such as QT/QML on ARM iMX6 Sabre SD.

We develop QT/QML applications for iMX6 platform and sometimes we feel that the debugging process will be much faster using a trace tool or something similar. My doubt is if the QT Creator gives support to this kind of hardware debugging tool or other that I didn't mentioned.

Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,480件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

seems GDB is native debugger according to

http://doc.qt.io/qtcreator/creator-debugging.html

http://doc.qt.io/qtcreator/creator-debugger-engines.html

also one can look at time storm plugins described on p.32

http://www.nxp.com/files/training/doc/dwf/DWF13_AMF_IND_T0847.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,481件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

seems GDB is native debugger according to

http://doc.qt.io/qtcreator/creator-debugging.html

http://doc.qt.io/qtcreator/creator-debugger-engines.html

also one can look at time storm plugins described on p.32

http://www.nxp.com/files/training/doc/dwf/DWF13_AMF_IND_T0847.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信