iMX6 - MFG-Tool firmware u-boot compiled in plugin mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 - MFG-Tool firmware u-boot compiled in plugin mode

2,345 Views
Ansari
Contributor IV

Hi,


We are using imx6Q our custom platform based on sabresd platform for our development with Linux 3.10.17_1.0.0-GA BSP.

Currently we are trying to program the binaries using "imx-3.10.17-1.0.2-mfg-tools" MFG-Tool.



We would like to know, Is it possible to use firmware (of MFG-tool) u-boot.imx in plugin mode?  or should we compile the MFG-Tool firmware u-boot binary in DCD mode?

Since our working u-boot.imx file is in plugin mode only.



Thank You,

Regards,

Ansari



0 Kudos
Reply
1 Reply

1,463 Views
igorpadykov
NXP Employee
NXP Employee

Hi Abdul

I think it may be used in both modes, if properly compiled.

May be recommended to check EB803 and

uboot-imx.git - Freescale i.MX u-boot Tree

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply