iMX6 HDMI volume control on R13.4.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 HDMI volume control on R13.4.1

2,281 Views
omar_ccc
Contributor II

We are using iMX6 running with SDK R13.4.1.

When we adjust the audio volume of HDMI output from Android Setting,  audio volume does not change.

Labels (2)
0 Kudos
Reply
2 Replies

1,692 Views
jamesbone
NXP TechSupport
NXP TechSupport

Unfortunately this release has several erratas or bugs with the HDMI port

ENGR00178468. HDMI Audio sometimes underrun! and then TV no music output mode 720P after switch different sample rate. 50%

ENGR00178531. HDMI audio played format is too few

ENGR00179425. Sometime HDMI mode is wrong and audio device gottend is wrong

0 Kudos
Reply

1,692 Views
weikeng-jimmy
Contributor III

Hi James,

Have you the fix patches for the three bugs ?  Thanks!

0 Kudos
Reply