iMX6 - GPT - linux kernel 3.0.35

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 - GPT - linux kernel 3.0.35

3,574 Views
davide_beretta
Contributor I

Hi everybody,

in my application I want to use the General Purpose Timer (GPT) of i.MX6Q but it is already configured and used for a delay routine in the kernel 3.0.35.

Is there a way to avoid the kernel to use GPT ?

thank you

Labels (2)
3 Replies

2,593 Views
fredo61
Contributor I

Hello Davide,

how did you manage to use the GPT?

Have you configured a second timer?

Fred

0 Kudos
Reply

2,593 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, Davide

     GPT is used for system clock source for kernel, so you can NOT touch it, all system time and broadcast timer are from GPT. You can try using EPIT, there are EPITs not used currently. Can I know what do you want to use GPT, to be a timer or counter?

2,593 Views
davide_beretta
Contributor I

I would like to use it as a counter.

Thank you.

0 Kudos
Reply