iMX6 - GPT - linux kernel 3.0.35

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 - GPT - linux kernel 3.0.35

3,532件の閲覧回数
davide_beretta
Contributor I

Hi everybody,

in my application I want to use the General Purpose Timer (GPT) of i.MX6Q but it is already configured and used for a delay routine in the kernel 3.0.35.

Is there a way to avoid the kernel to use GPT ?

thank you

ラベル(2)
3 返答(返信)

2,551件の閲覧回数
fredo61
Contributor I

Hello Davide,

how did you manage to use the GPT?

Have you configured a second timer?

Fred

0 件の賞賛
返信

2,551件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Hi, Davide

     GPT is used for system clock source for kernel, so you can NOT touch it, all system time and broadcast timer are from GPT. You can try using EPIT, there are EPITs not used currently. Can I know what do you want to use GPT, to be a timer or counter?

2,551件の閲覧回数
davide_beretta
Contributor I

I would like to use it as a counter.

Thank you.

0 件の賞賛
返信