iMX6 - GPT - linux kernel 3.0.35

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6 - GPT - linux kernel 3.0.35

3,624 次查看
davide_beretta
Contributor I

Hi everybody,

in my application I want to use the General Purpose Timer (GPT) of i.MX6Q but it is already configured and used for a delay routine in the kernel 3.0.35.

Is there a way to avoid the kernel to use GPT ?

thank you

标签 (2)
3 回复数

2,643 次查看
fredo61
Contributor I

Hello Davide,

how did you manage to use the GPT?

Have you configured a second timer?

Fred

0 项奖励
回复

2,643 次查看
AnsonHuang
NXP Employee
NXP Employee

Hi, Davide

     GPT is used for system clock source for kernel, so you can NOT touch it, all system time and broadcast timer are from GPT. You can try using EPIT, there are EPITs not used currently. Can I know what do you want to use GPT, to be a timer or counter?

2,643 次查看
davide_beretta
Contributor I

I would like to use it as a counter.

Thank you.

0 项奖励
回复