iMX6 DDR3 Address Line Layout

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 DDR3 Address Line Layout

1,264 Views
massimomantovan
Contributor I

Hi, 

I'm trying to route a T-Branch topology Address Line on iMX6Q.

The board will be little, and I use 12 layer stack up, (4 sig. layer, 4 gnd layer, 4 Pw layer).

I would like to try to route all the add/cmd signals on an inner layer, but I should have a lot of space between memories chip.

 

I noted that in the evaluation board MCIMX6Q-SBD the address line it has been divided on two layers. (half line on bottom layer and half on inner layer I do not remember which one).

Could it be a good solution? 

Thanks!

Massimo 

Tags (1)
1 Reply

1,185 Views
igorpadykov
NXP Employee
NXP Employee

Hi Massimo

general layout rules are described in i.MX6 System Development User’s Guide

and I think your solution also can be used.

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------