iMX6 Boot Pin configuration, USB OTG

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6 Boot Pin configuration, USB OTG

1,841 次查看
enriqueencarnac
Contributor II

Hello,

When I designed my IMX6 board I made the USB OTG port permanently configured to be a host, as this is how it will be used in our product.

In bringing up the board I see that the i.MX6 uses this port in OTG mode to make the board a device and to be able to download the bootloader using this USB port.

I would like to confirm that if the BOOT PINS are configured as BOOT [1:0] = 10 and the rest of the boot cfg pins are set to boot from SD Card that we should still be able to compile and build an image that can be executed from the SD Card?

标签 (4)
0 项奖励
回复
1 回复

1,447 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Enrique

right, with BOOT [1:0] = 10 and other boot cfg pins set to boot from SD

image will be executed from the SD Card.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复