iMX6 Bare-Metal SMP Debugging using DS-5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 Bare-Metal SMP Debugging using DS-5

ソリューションへジャンプ
2,695件の閲覧回数
jonathanblancha
Contributor I

Contrary to the multiple cpus I've used with DS-5 the iMX6Q always shows core 1-3 as being powered down. Anyone been able to get DS-5 to connect to all four cores?

For reference I'm using the iMX6 SABRE dev board and DS-5 5.18 pro.

Jonathan

ラベル(1)
0 件の賞賛
返信
1 解決策
2,194件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jonathan

by default cores 1-3 are disabled, there is special procedure to

run them. Please look at description and example codes in SDK

Chapter 3 Multicore Startup.

"MX6_PLATFORM_SDK "

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&nodeId=018rH3ZrDRB24A&fpsp=1&t...

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,195件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jonathan

by default cores 1-3 are disabled, there is special procedure to

run them. Please look at description and example codes in SDK

Chapter 3 Multicore Startup.

"MX6_PLATFORM_SDK "

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&nodeId=018rH3ZrDRB24A&fpsp=1&t...

0 件の賞賛
返信
2,194件の閲覧回数
jonathanblancha
Contributor I

Hi again,

As a reference for anyone else trying to do the same thing powering up the cores after the debug session is started won't enable debugging on those cores meaning that breakpoints and semi hosting won't work. Recommended approach is to let a bootloader or a debug script do the multi core init.

Jonathan Blanchard

0 件の賞賛
返信