iMX6 Android - HWcomposer problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 Android - HWcomposer problem

Jump to solution
7,414 Views
udoschmelmer
Contributor II

Hello,

while working on an android port for a imx6q custom board i am facing a problem with the hardwarecomposer.

This is the logcat output:

--------- beginning of /dev/log/main

I/installd( 2030): installd firing up

D/        ( 2033): init_sensors

E/cutils  ( 2030): Failed to read /data/.layout_version: No such file or directory

D/installd( 2030): Upgrading /data/media for multi-user

E/cutils  ( 2030): Failed to chown(/data/media/, 1023, 1023): Operation not permitted

E/installd( 2030): Could not create directories; exiting.

I/DEBUG   ( 2024): debuggerd: Aug 27 2013 10:39:06

--------- beginning of /dev/log/system

I/Vold    ( 2021): Vold 2.1 (the revenge) firing up

D/        ( 2033): couldn't find 'mma845x' input device

D/MagDaemon( 2033): inital sensor error

D/Vold    ( 2021): Volume udisk state changing -1 (Initializing) -> 0 (No-Media)

D/Vold    ( 2021): Volume extsd state changing -1 (Initializing) -> 0 (No-Media)

I/Netd    ( 2023): Netd 1.0 starting

W/InterfaceController( 2023): Warning (Cannot load library: load_library(linker.cpp:745): library "/system/lib/libnetcmdiface.so" not found) while opening the net interface command library

I/SurfaceFlinger( 2025): SurfaceFlinger is starting

I/SurfaceFlinger( 2025): SurfaceFlinger's main thread ready to run. Initializing graphics H/W...

D/libEGL  ( 2025): loaded /system/lib/egl/libEGL_VIVANTE.so

D/libEGL  ( 2025): loaded /system/lib/egl/libGLESv1_CM_VIVANTE.so

D/libEGL  ( 2025): loaded /system/lib/egl/libGLESv2_VIVANTE.so

W/imx6.gralloc( 2025): 32bpp setting of Framebuffer catched!

W/imx6.gralloc( 2025): using (fd=16)

W/imx6.gralloc( 2025): id           = DISP3 BG

W/imx6.gralloc( 2025): xres         = 800 px

W/imx6.gralloc( 2025): yres         = 480 px

W/imx6.gralloc( 2025): xres_virtual = 800 px

W/imx6.gralloc( 2025): yres_virtual = 1536 px

W/imx6.gralloc( 2025): bpp          = 32

W/imx6.gralloc( 2025): r            =  0:8

W/imx6.gralloc( 2025): g            =  8:8

W/imx6.gralloc( 2025): b            = 16:8

W/imx6.gralloc( 2025): width        = 127 mm (160.000000 dpi)

W/imx6.gralloc( 2025): height       = 76 mm (160.421051 dpi)

W/imx6.gralloc( 2025): refresh rate = 59.48 Hz

I/FslHwcomposer( 2025): fb0 is ldb

I/FslHwcomposer( 2025):  device

I/FslHwcomposer( 2025): fb1 is overlay device

I/FslHwcomposer( 2025): fb2 is hdmi

I/FslHwcomposer( 2025):  device

I/FslHwcomposer( 2025): open /sys/class/graphics/fb2/disp_dev/cable_state failed

W/FslHwcomposer( 2025): system can't support more than 2 devices

I/FslHwcomposer( 2025): hwcomposer: open framebuffer fb0

I/v_hwc   ( 2025): Detected display /dev/graphics/fb0

I/v_hwc   ( 2025): xres         = 800 px

I/v_hwc   ( 2025): yres         = 480 px

I/v_hwc   ( 2025): xres_virtual = 800 px

I/v_hwc   ( 2025): yres_virtual = 1536 px

I/v_hwc   ( 2025): width        = -1 mm (0.0 dpi)

I/v_hwc   ( 2025): height       = -1 mm (0.0 dpi)

I/v_hwc   ( 2025): refresh rate = 59.0 Hz

I/v_hwc   ( 2025): Detected display /dev/graphics/fb2

I/v_hwc   ( 2025): xres         = 640 px

I/v_hwc   ( 2025): yres         = 480 px

I/v_hwc   ( 2025): xres_virtual = 640 px

I/v_hwc   ( 2025): yres_virtual = 480 px

I/v_hwc   ( 2025): width        = -1 mm (0.0 dpi)

I/v_hwc   ( 2025): height       = -1 mm (0.0 dpi)

I/v_hwc   ( 2025): refresh rate = 60.0 Hz

E/v_hwc   ( 2025): hwc_device_open(345): Failed to initialize hwcomposer!

E/FslHwcomposer( 2025): Error! viv_hwc open failed

I/FslHwcomposer( 2025): hwc_device_open,367

I/SurfaceFlinger( 2025): Using composer version 1.1

W/SurfaceFlinger( 2025): no suitable EGLConfig found, trying without EGL_FRAMEBUFFER_TARGET_ANDROID

W/SurfaceFlinger( 2025): no suitable EGLConfig found, trying without EGL_RECORDABLE_ANDROID

W/SurfaceFlinger( 2025): no suitable EGLConfig found, trying with 16-bit color allowed

E/SurfaceFlinger( 2025): no suitable EGLConfig found, giving up

E/libEGL  ( 2025): validate_display_connection:266 error 3005 (EGL_BAD_CONFIG)

F/libc    ( 2025): Fatal signal 11 (SIGSEGV) at 0x00000004 (code=1), thread 2062 (SurfaceFlinger)

I/DEBUG   ( 2024): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***

I/DEBUG   ( 2024): Build fingerprint: 'Freescale/sabresd_6dq/sabresd_6dq:4.2.2/1.0.0-rc3/eng.*****.20130827.103040:eng/dev-keys'

I/DEBUG   ( 2024): Revision: '99'

I/DEBUG   ( 2024): pid: 2025, tid: 2062, name: SurfaceFlinger  >>> /system/bin/surfaceflinger <<<

I/DEBUG   ( 2024): signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr 00000004

-------------------------

my bootargs:

bootargs=console=ttymxc0,115200 root=/dev/nfs ip=dhcp nfsroot=10.0.150.1:/home/pxeroot/android/rootfs,v3,tcp video=mxcfb0:dev=ldb,800x480M@60,if=RGB666 ldb=sin0 androidboot.hardware=freescale init=/init vmalloc=400M fbmem=28M rw

------------------------

It seems as the problem sits somewhere around system/lib/hw/hwcomposer_viv.imx6.so

The kernel is booting up nicely and is showing all four penguins.

I am new in this field and would be very grateful for any advice where i can start from.

Thanks,

Udo Schmelmer

Labels (4)
0 Kudos
Reply
1 Solution
4,006 Views
udoschmelmer
Contributor II

Hi Yixing,

i got it managed. I used a too old version of the kerneldriver. After updating it worked fine!

You can close the discussion.

Thanks,

Udo

View solution in original post

0 Kudos
Reply
2 Replies
4,006 Views
YixingKong
Senior Contributor IV

Udo

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the

issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.

Thanks,
Yixing

0 Kudos
Reply
4,007 Views
udoschmelmer
Contributor II

Hi Yixing,

i got it managed. I used a too old version of the kerneldriver. After updating it worked fine!

You can close the discussion.

Thanks,

Udo

0 Kudos
Reply