iMX6 Android 4.2.2 HDMI problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 Android 4.2.2 HDMI problem

3,190件の閲覧回数
ppatierno
Contributor I

Hello,

I downloaded android_jb4.2.2_1.1.0 with all source code and

patches and I built an image for our Sabre SDB board.

I changed the kernel command line in this way :

BOARD_KERNEL_CMDLINE := console=ttymxc0,115200

androidboot.console=ttymxc0 vmalloc=400M init=/init

video=mxcfb0:dev=hdmi,1920x1080M@60 video=mxcfb1:off

video=mxcfb2:off androidboot.hardware=freescale fbmem=28M

to support HDMI video (not LVDS as default command line in the

same file).

When operating system starts, kernel boots and Android boots

but on the display the image is as picture atteched.

Why ?

Thanks,

Paolo Patierno

ラベル(6)
タグ(2)
0 件の賞賛
返信
1 返信

2,074件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi,

I can not see the kind of Monitor you are using but it looks like the resolution is not suitable for it. However, pleae try this steps in another hdmi monitor to make sure it works.

In the U-Boot prompt, set the U-Boot environment variables as shown below:

U-Boot > setenv bootcmd booti mmc3

U-Boot > setenv bootargs console=ttymxc0,115200 androidboot.console=ttymxc0 vmalloc=400M

init=/init video=mxcfb0:dev=hdmi,1920x1080M@60,bpp=32 video=mxcfb1:off video=mxcfb2:off

fbmem=28M androidboot.hardware=freescale

U-Boot > saveenv

Regards

0 件の賞賛
返信