iMX535 Quick Start Board - Changing Mac Address

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX535 Quick Start Board - Changing Mac Address

1,672件の閲覧回数
neeveehariharan
Contributor I

Hi,

iMX535 based Quick Start board contains the MAC Address information is stored in IIM ( IC Identification Module ) fuses. U-boot has been provided with the following commands to change the mac address but the change is not effective.

"iim blow fecmac" command.

Advance thanks for your valuable inputs.

Thanks,

Hariharan.V.

NEE VEE Communication Technologies ( www.neeveetech.com )

タグ(1)
0 件の賞賛
返信
1 返信

1,454件の閲覧回数
neeveehariharan
Contributor I

Hi,

iMX535 processor contains VDD_FUSE pin should be 3.2V for IIM Fuse Bits programming.

Configure of LDO of PMIC of ( DS9503 / LTC3589-1), provides the respective voltage.

Thanks,

Hariharan.V.

0 件の賞賛
返信