iMX535 Quick Start Board - Changing Mac Address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX535 Quick Start Board - Changing Mac Address

1,657 Views
neeveehariharan
Contributor I

Hi,

iMX535 based Quick Start board contains the MAC Address information is stored in IIM ( IC Identification Module ) fuses. U-boot has been provided with the following commands to change the mac address but the change is not effective.

"iim blow fecmac" command.

Advance thanks for your valuable inputs.

Thanks,

Hariharan.V.

NEE VEE Communication Technologies ( www.neeveetech.com )

Tags (1)
0 Kudos
Reply
1 Reply

1,439 Views
neeveehariharan
Contributor I

Hi,

iMX535 processor contains VDD_FUSE pin should be 3.2V for IIM Fuse Bits programming.

Configure of LDO of PMIC of ( DS9503 / LTC3589-1), provides the respective voltage.

Thanks,

Hariharan.V.

0 Kudos
Reply