iMX535 Quick Start Board - Changing Mac Address

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX535 Quick Start Board - Changing Mac Address

1,636 次查看
neeveehariharan
Contributor I

Hi,

iMX535 based Quick Start board contains the MAC Address information is stored in IIM ( IC Identification Module ) fuses. U-boot has been provided with the following commands to change the mac address but the change is not effective.

"iim blow fecmac" command.

Advance thanks for your valuable inputs.

Thanks,

Hariharan.V.

NEE VEE Communication Technologies ( www.neeveetech.com )

标记 (1)
0 项奖励
回复
1 回复

1,418 次查看
neeveehariharan
Contributor I

Hi,

iMX535 processor contains VDD_FUSE pin should be 3.2V for IIM Fuse Bits programming.

Configure of LDO of PMIC of ( DS9503 / LTC3589-1), provides the respective voltage.

Thanks,

Hariharan.V.

0 项奖励
回复