iMX535 IBIS Models

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX535 IBIS Models

2,993 Views
sherry_zahid
Contributor III

Hi,

I require the latest IBIS models for iMX535 (19x19mm). I need this to run simulations for verifying DDR3 signal integrity. Does the iMX535 have IBIS models that include the DDR3 pins with a 120ohm ODT set up? 

Thanks

Labels (1)
0 Kudos
Reply
3 Replies

2,802 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Sherry,

In the following link you can download the IBIS Model.

i.MX537 Processors|HD Video|NXP 

Best Regards,

Jaime

0 Kudos
Reply

2,799 Views
jagdish_goswami
Contributor I

Hi,

I am also in need of the IBIS model of IMX535DVV1C.

I searched the link Shared above by jamesbone‌ 

But couldn't find it there.

Can you please help me in getting the IBIS model?

I need to perform the Signal integrity Analysis of DDR2 interface.

0 Kudos
Reply

2,799 Views
sherry_zahid
Contributor III

Thanks! I am guessing this is the latest available version? In regard to the IBIS models, would you be able to outline the difference between IBIS models that use a "Driver impedance" and "ODT (on-die termination)"? How are these termination schemes different? 

Regards

0 Kudos
Reply