iMX535 Fuse Setting boot MMU enabled with security open

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX535 Fuse Setting boot MMU enabled with security open

Jump to solution
2,316 Views
sherry_zahid
Contributor III

Question on the subject of iMX535 fuses:

Would the following fuse settings result in any issues / problems / risks?
If boot MMU/Cache is enabled (BT_MMU_ENABLE=1) but security config is left open (SEC_CONFIG=01)

Additional info:
Setting up to boot via eMMC

BT_MMU_ENABLE IIM address:080C[0]

SEC_CONFIG IIM address:0810[1:0]

Thanks

SZ

Labels (1)
0 Kudos
Reply
1 Solution
2,096 Views
igorpadykov
NXP Employee
NXP Employee

Hi sherry

 

there is no special technical reason for the above recommendation,

it just points that with SEC_CONFIG=Open this setting is useless, 

as will not improve boot performance.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
3 Replies
2,096 Views
igorpadykov
NXP Employee
NXP Employee

Hi sherry

no, it will not cause any problems or issues

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,096 Views
sherry_zahid
Contributor III

Hi Igor,

 

Thanks for the quick response. The reason I asked was because the reference manual recommends that boot MMU/cache should be disabled if security config is left open:-


From IMX53RM Rev2.1 (Section 7.4.4)

"Enabling the MMU when booting non-securely by setting, SEC_CONFIG=Open and
setting the CSF pointer in the Image Vector Table set to NULL, has no impact on the
boot performance. With this configuration it is recommended not to blow the MMU_EN
fuse."

 

Would there be any technical reason for the above recommendation? 

 

Thanks,

SZ

0 Kudos
Reply
2,097 Views
igorpadykov
NXP Employee
NXP Employee

Hi sherry

 

there is no special technical reason for the above recommendation,

it just points that with SEC_CONFIG=Open this setting is useless, 

as will not improve boot performance.

 

Best regards
igor

0 Kudos
Reply