iMX535 Fuse Setting boot MMU enabled with security open

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX535 Fuse Setting boot MMU enabled with security open

跳至解决方案
2,314 次查看
sherry_zahid
Contributor III

Question on the subject of iMX535 fuses:

Would the following fuse settings result in any issues / problems / risks?
If boot MMU/Cache is enabled (BT_MMU_ENABLE=1) but security config is left open (SEC_CONFIG=01)

Additional info:
Setting up to boot via eMMC

BT_MMU_ENABLE IIM address:080C[0]

SEC_CONFIG IIM address:0810[1:0]

Thanks

SZ

标签 (1)
0 项奖励
回复
1 解答
2,094 次查看
igorpadykov
NXP Employee
NXP Employee

Hi sherry

 

there is no special technical reason for the above recommendation,

it just points that with SEC_CONFIG=Open this setting is useless, 

as will not improve boot performance.

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,094 次查看
igorpadykov
NXP Employee
NXP Employee

Hi sherry

no, it will not cause any problems or issues

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,094 次查看
sherry_zahid
Contributor III

Hi Igor,

 

Thanks for the quick response. The reason I asked was because the reference manual recommends that boot MMU/cache should be disabled if security config is left open:-


From IMX53RM Rev2.1 (Section 7.4.4)

"Enabling the MMU when booting non-securely by setting, SEC_CONFIG=Open and
setting the CSF pointer in the Image Vector Table set to NULL, has no impact on the
boot performance. With this configuration it is recommended not to blow the MMU_EN
fuse."

 

Would there be any technical reason for the above recommendation? 

 

Thanks,

SZ

0 项奖励
回复
2,095 次查看
igorpadykov
NXP Employee
NXP Employee

Hi sherry

 

there is no special technical reason for the above recommendation,

it just points that with SEC_CONFIG=Open this setting is useless, 

as will not improve boot performance.

 

Best regards
igor

0 项奖励
回复