iMX53 choose boot from which mmc interface?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX53 choose boot from which mmc interface?

2,516 Views
JayZhang
Contributor I

Is there a GPIO pin that can choose which mmc interface to boot up ?

Sorry for my poor English and thanks for your suggest!

Labels (1)
0 Kudos
Reply
6 Replies

2,251 Views
JayZhang
Contributor I

Hy,

Thanks a lot.

xizhou wang said:

FYI

 

Comment by Mark Middletonon November 28, 2011 at 10:40am

To boot from SD3 (Full size SD Card socket), the "short" answer is to solder a wire between pads 2 & 19 of SW1. See picture. For more detail, see section 5.4.2 of the HW User Guide. The SW1 footprint was designed for a Multicomp MCNHDS-10-T Dip switch.

211-INST.JPG

0 Kudos
Reply

2,251 Views
xizhouwang
Contributor II

FYI

 

Comment by Mark Middletonon November 28, 2011 at 10:40am

To boot from SD3 (Full size SD Card socket), the "short" answer is to solder a wire between pads 2 & 19 of SW1. See picture. For more detail, see section 5.4.2 of the HW User Guide. The SW1 footprint was designed for a Multicomp MCNHDS-10-T Dip switch.

213-INST.JPG

0 Kudos
Reply

2,251 Views
Yuri
NXP Employee
NXP Employee

SD port select option BOOT_CFG3[5:4] (EIM_DA6, EIM_DA7) may be configured on (BOOT) SW1
of the QSB. Please use the scheme for details.
Also one may look at section 5.5.2 (Boot Mode Operations and Selections)
of “Hardware Reference Manual for i.MX53 Quick Start”.

0 Kudos
Reply

2,251 Views
KrishnaPavan
Contributor II

Hi Yuri Mihin,

What about the DIP Switches, that are used in general then?

What should be the state of them, If we use GPIO Pins directly?

0 Kudos
Reply

2,251 Views
Yuri
NXP Employee
NXP Employee

According to Table 7-15 (ESDHC Boot eFUSE Descriptions) of i.MX53 Reference
Manual (RM), BOOT_CFG3[5:4] fuses are responsible for SD port selection.

Table 7-3 (GPIO Override Contact Assignments) of the RM shows what pins
may be used instead of fuses.

 

http://cache.freescale.com/files/32bit/doc/ref_manual/iMX53RM.pdf 

0 Kudos
Reply

2,251 Views
JayZhang
Contributor I

Any one can help me?

0 Kudos
Reply