iMX53 UART data lost when receiving

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX53 UART data lost when receiving

1,162件の閲覧回数
charleshuang
Senior Contributor II

Hi,

Is there any theory to explain why data lost when receiving.

TEST : (10 times)

Rx(iMX53)

# stty -F /dev/ttymxc2 speed 115200 -echo

# cat /dev/ttymxc2 > result.txt

Tx(PC): transfer one text file that contains 10000 characters.

FAILED : The size of result.txt is about 2000 ~ 4000 bytes.

ラベル(2)
0 件の賞賛
返信
1 返信

1,065件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi charles

data may be lost due to UART RX buffer overflow,

since processor is busy on other tasks.

One can try to decrease processor load or try to use SDMA

with UART (this may alleviate problem but may not provide full guarantee).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信