iMX53 NAND NFC Kernel support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX53 NAND NFC Kernel support

ソリューションへジャンプ
3,387件の閲覧回数
bdp42
Contributor IV

Hi,

I have a simple question about the correct kernel config option for iMX53 NAND NFC support. Should CONFIG_MTD_NAND_IMX_NFC should be enabled in the kernel?

The reason I ask is that the imx5_defconfig file (which supports MX53 NAND) does not have it set yet it looks like it should be set. Here's the relevant piece of the config file

  • #
  • # Disk-On-Chip Device Drivers
  • #
  • # CONFIG_MTD_DOC2000 is not set
  • # CONFIG_MTD_DOC2001 is not set
  • # CONFIG_MTD_DOC2001PLUS is not set
  • CONFIG_MTD_NAND=y
  • # CONFIG_MTD_NAND_VERIFY_WRITE is not set
  • # CONFIG_MTD_NAND_ECC_SMC is not set
  • # CONFIG_MTD_NAND_MUSEUM_IDS is not set
  • # CONFIG_MTD_NAND_GPIO is not set
  • CONFIG_MTD_NAND_IDS=y
  • # CONFIG_MTD_NAND_DISKONCHIP is not set
  • # CONFIG_MTD_NAND_NANDSIM is not set
  • # CONFIG_MTD_NAND_IMX_NFC is not set
  • CONFIG_MTD_NAND_MXC_V3=y
  • # CONFIG_MTD_NAND_MXC_SWECC is not set
  • # CONFIG_MTD_NAND_MXC_FORCE_CE is not set
  • # CONFIG_MXC_NAND_LOW_LEVEL_ERASE is not set
  • # CONFIG_MTD_NAND_PLATFORM is not set
  • # CONFIG_MTD_ALAUDA is not set
  • # CONFIG_MTD_ONENAND is not set

Can someone clarify this?

Thanks,

Bruno

ラベル(3)
0 件の賞賛
返信
1 解決策
3,126件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Bruno

CONFIG_MTD_NAND_IMX_NFC was

for older NFC revisions used in i.MX21,MX31.


Best regards

igor

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,124件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Bruno

I believe not since one has already CONFIG_MTD_NAND_MXC_V3=y,

also refer to attached file. In ltib build one can select ard board,

it has nand support

L2.6.35_11.05_ER_SOURCE : Linux 2.6.35 Source Code Files and documentation 11.05 for i.MX53 SABRE Tablet.

Best regards

igor

0 件の賞賛
返信
3,124件の閲覧回数
bdp42
Contributor IV

Hi Igor,

OK. It looks like CONFIG_MTD_NAND_MXC_V3=y is the correct configuration option to use the iMX53 NAND Flash Controller.

I'm just curious what CONFIG_MTD_NAND_IMX_NFC  is used for?


Bruno

0 件の賞賛
返信
3,127件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Bruno

CONFIG_MTD_NAND_IMX_NFC was

for older NFC revisions used in i.MX21,MX31.


Best regards

igor

0 件の賞賛
返信