iMX53 DMA Issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX53 DMA Issues

1,636 Views
fraserwinters
Contributor I

I am currently developing a new system based on the iMX53 device and using Linux 2.6.35. We have three UART connections to this system running at a relatively high speed (921kbaud) and have issues trying to get this running with DMA enabled for the three UARTS. We have inconsistent results in DMA mode with what appears to be bytes dropped, delayed interrupts depending on the message and channel and various other issues.

I have tried applying the patch for the DMA micro code which did not appear to resolve the issues. On a post I found there was mention of Freescale support having an updated mxc_uart.c with updates for DMA operation. Does anyone know where this update is available or do they have it and could supply a copy?

At present we are running without DMA which is obviously not ideal due to high number of interrupts and the occassional OE error we encounter...

Is anyone aware of any further updates for DMA microcode.

For reference we are not using a Freescale BSP due to the board we are using although obviously most of the files for the driver layer are the Freescale versions.

Thanks

Fraser

Labels (2)
0 Kudos
Reply
1 Reply

1,466 Views
Yuri
NXP Employee
NXP Employee

Perhaps, it may be useful to look at the following patches 

from the git, linked below.

ENGR00252150 Fix MX53 IOMUX setup for all UARTsimx_2.6.35_11.09.01   

ENGR40066538-3 MX53: UART: enable the hardware flow control

ENGR40066538-2 MX53: UART: fix the wrong CTS pinmux macro   

ENGR40066538-1 MX53: UART: update the DMA script for UART   

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_2.6.35_11.09.01


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply