iMX51 EVK Lucid (Demo Image) OpenCV Build Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX51 EVK Lucid (Demo Image) OpenCV Build Error

1,615件の閲覧回数
PrachiSinghal
Contributor I

Hi,

I am following the following link to build and install EmguCV on Linux (9.04 Lucid Demo Image from Freescale) on iMX51 EVK board.
http://www.emgu.com/wiki/index.php/Down ... tion#Linux

Please note that EmguCV mentions the custom install of OpenCV and instructs to remove any OpenCV version installed on OS. So, I didn`t think building of OpenCV on iMX51 EVK as mentioned on http://www.imxdev.org/wiki/index.php?title=I.MX51_EVK_Board_OpenCV

After step 3 (generating the makefile), when i execute `make` command, I am getting the error logs (file attached). The build process terminates with the following error:

c++: Internal error: Segmentation fault (program cc1plus)

Please submit a full bug report.

See <file:///usr/share/doc/gcc-4.4/README.Bugs> for instructions.

 

I also tried re-installing g++

sudo apt-get -–reinstall install g++-4.4

But this didn`t help. I am getting the same error repeatedly, though at different files each time.

 

Please experts... give some possible suggestions to resolve this.

 

Thank you.

ラベル(1)
タグ(2)
0 件の賞賛
返信
0 返答(返信)