iMX51: Build Android Image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX51: Build Android Image

Jump to solution
2,716 Views
brianlin
Contributor II

Hi all,

Please help me. I am building Android image for iMX51. But found below error message. How can I do now? Thanks.

test-host@test-host:~/Downloads/myandroid$ make

============================================

PLATFORM_VERSION_CODENAME=REL

PLATFORM_VERSION=2.3.7

TARGET_PRODUCT=mx51

TARGET_BUILD_VARIANT=eng

TARGET_SIMULATOR=false

TARGET_BUILD_TYPE=release

TARGET_BUILD_APPS=

TARGET_ARCH=arm

HOST_ARCH=x86

HOST_OS=linux

HOST_BUILD_TYPE=release

BUILD_ID=GWK74

============================================

find: `frameworks/base/frameworks/base/docs/html': No such file or directory

find: `out/target/common/docs/gen': No such file or directory

find: `frameworks/base/frameworks/base/docs/html': No such file or directory

find: `out/target/common/docs/gen': No such file or directory

find: `frameworks/base/frameworks/base/docs/html': No such file or directory

find: `out/target/common/docs/gen': No such file or directory

find: `frameworks/base/frameworks/base/docs/html': No such file or directory

find: `out/target/common/docs/gen': No such file or directory

find: `frameworks/base/frameworks/base/docs/html': No such file or directory

find: `out/target/common/docs/gen': No such file or directory

device/fsl/mx51/AndroidBoard.mk:6: warning: overriding commands for target `out/target/product/mx51/system/usr/keylayout/tuttle2.kl'

device/fsl/mx51/AndroidBoard.mk:6: warning: ignoring old commands for target `out/target/product/mx51/system/usr/keylayout/tuttle2.kl'

build/core/base_rules.mk:162: *** device/fsl/mx51: MODULE.TARGET.KEYCHARS.tuttle2.kcm already defined by device/fsl/mx51.  Stop.


Labels (3)
0 Kudos
Reply
1 Solution
2,032 Views
jimmychan
NXP TechSupport
NXP TechSupport

Command to build for i.MX51 BBG 3.0 board is:

    $ source build/envsetup.sh 

    $ lunch imx51_bbg-user

    $ make

    "imx51_bbg" is the product names (see ~/myandroid/device/fsl/product)

View solution in original post

0 Kudos
Reply
1 Reply
2,033 Views
jimmychan
NXP TechSupport
NXP TechSupport

Command to build for i.MX51 BBG 3.0 board is:

    $ source build/envsetup.sh 

    $ lunch imx51_bbg-user

    $ make

    "imx51_bbg" is the product names (see ~/myandroid/device/fsl/product)

0 Kudos
Reply