Hi
We managed to capture images after we changed the IO voltage to 2.8V ...
We now have a problem with high resolution capture... we have written a driver for working in linux 2.6.24 for using the same for our capture and view application.
We are able to achieve 2048x1536 resolution in mxc_v4l2_overlay application and also able to view the full image on the LCD. But the observation is that the in the same mode - 2048x1536, when we try for still image capture using mxc_v4l2_still application, we find that the mxc_v4l2_read error is coming. Can you let us know if there is anything that we can do to get around this problem?
Thanks and best regards