iMX28X_EVK board not detecting in Windows 7 64-bit System

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX28X_EVK board not detecting in Windows 7 64-bit System

901件の閲覧回数
bkpatel
Contributor III

Hi,

I am trying to connect my iMX28 board with windows 7 64-bit system but device is not showing in Device Manager.

While connecting to Windows 8 it is showing under Human Interface Device (HID) List. Same is not available in Windows7.

How to connect to Windows 7?

Want to upload kernel and rootfs via MfgTool.

Thanks,

Bhavesh

ラベル(3)
0 件の賞賛
返信
1 返信

710件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Bhavesh

please try solutions provided on

Mfgtool can't connect in windows7

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信