iMX287 running on external oscillator?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX287 running on external oscillator?

1,928 次查看
albertguardiola
Contributor III

Hi all,

Is it possible to make the iMX work with external oscillator (not crystal)? We are discussing this alternative because integrated oscillators offer much better MTBF values than crystals. (20 times better!)

If not, can we run the iMX (including the RTC subcircuit) only with the internal oscillator?

Bets regards

4 回复数

1,768 次查看
Yuri
NXP Employee
NXP Employee

I am afraid, we have no any specifications for using external clock sources,

except crystals, with i.MX28.  The only recommendations are to use 24MHz, 30ppm

Crystal, and 32kHz, 20ppm Crystal.

More details for 24Mhz :

+/- 30ppm ;

max ESR: ~50ohm ;

Load capacitor : 10pf-15pf ;

Shunt capacitor : 5pf-7pf.

  Sorry, an external oscillator option has never been tested with i.MX28.

Theoretically, it seems to be possible to apply an external 24MHz clock signal

to XTALI and leave XTALO open, however, the amplitude of an external clock

signal must not exceed VDDXTAL, that is typically around 1.0V.


The internal oscillator may be used in low power mode. By default it is disabled.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,768 次查看
albertguardiola
Contributor III

Thanks indeed, Yuri,

How about running the whole IMX on internal oscillator? Is there any limitation in functionality?

I cannot find literature on the internal oscillator in the datasheets: could you provide quality specs on it?

Best regards

0 项奖励
回复

1,768 次查看
Yuri
NXP Employee
NXP Employee

The internal oscillator may be used in low power mode. By default it is disabled.

Regards,

Yuri.

1,768 次查看
albertguardiola
Contributor III

Thanks for the info, Yuri. Best regards.

0 项奖励
回复