unable to start bluetooth in kitkat 4.4.3 with imx6 sololite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

unable to start bluetooth in kitkat 4.4.3 with imx6 sololite

936 Views
mutyalaraoneela
Contributor III

Hi,

     I am completely new to bluedroid. I made some changes in init.rc file then i got bluetooth icon on my GUI.But if i am enabling bluetooth on GUI, interface not ready and error while setting the callbacks is showing in logcat.As per the code i had seen that it is calling the callbacks in the bluetooth.c file. Can anybody please help or guide us what to do?

Thanks in advance,

Mutyalarao.

Labels (3)
0 Kudos
Reply
1 Reply

716 Views
igorpadykov
NXP Employee
NXP Employee

Hi mutyalarao

for learning bluetooth one can start with links below

How to enable BT on i.MX 6SoloLite EVK Board

https://community.freescale.com/servlet/JiveServlet/previewBody/95006-102-1-6867/142-00207-517_iMX6X...

How to Enable USB Bluetooth Dongle Based on i.MX6 Android ICS

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply