iMX280 GPIO configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX280 GPIO configuration

824 次查看
manjunathdn
Contributor I

How can we drive the GPIO's of iMX280 to high impedance or tri-state? Can someone provide details of the GPIO configuration / settings?

标签 (1)
0 项奖励
回复
1 回复

747 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Manjunath

this is provided by HW_PINCTRL_DOEx register, from

sect.9.4.53 PINCTRL Bank 0 Data Output Enable Register

(HW_PINCTRL_DOE0) MCIMX28RM

For pins in bank 0 that are configured as GPIOs, a 1 in this register will enable the

corresponding bit value from HW_PINCTRL_DOUTxx register to be driven out the pin,

and a 0 in this register will disable the corresponding driver.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复